This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: TMS320C6657 DDR接口相关问题

Part Number: TMS320C6657


我们现在使用TMS320C6657进行设计,DDR3部份有以下问题需要咨询。

1.DDR3我们使用2Gb单片的型号,请问是否支持?请问有没有DDR3的支持表,还是市面上标准的DDR3都能支持?
2.我们使用2片16bit的DDR3,这里的DDRCLKOUT0和DDRCLKOUT1分别是连到2片DDR3上还是用DDRCLKOUT0一拖二?
3.我们使用2片16bit的DDR3,这里的DDRCKE0和DDRCKE1分别是连到2片DDR3上还是用DDRCLKOUT0一拖二?
4.我们使用2片16bit的DDR3,这里的DDRCE0和DDRCE1分别是连到2片DDR3上还是用DDRCLKOUT0一拖二?
5.我们使用2片16bit的DDR3,这里的DDRODT0和DDRODT1分别是连到2片DDR3上还是用DDRCLKOUT0一拖二?
6.我们的DDR3没有A15这个地址位,请问这个A15该如何连接? 可以悬空吗?
7.请问DDRDQM8,DDRDQS8P/N,DDRCB00/01/02/03这几个信号是什么信号? 该如何连接?