根据论坛中的解答EMU0和EMU1是双向信号
在EVM板原理图上使用usb转jtag的FTD2232HL芯片,然后再交给与非门输出EMU0和EMU1。在这个电路中EMU0和EMU1信号只能是输出信号,与非门决定。如何解释?是不是这种方式EMU0和EMU1只能是输出,即DSP的输入?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据论坛中的解答EMU0和EMU1是双向信号
在EVM板原理图上使用usb转jtag的FTD2232HL芯片,然后再交给与非门输出EMU0和EMU1。在这个电路中EMU0和EMU1信号只能是输出信号,与非门决定。如何解释?是不是这种方式EMU0和EMU1只能是输出,即DSP的输入?
是的,这种接法是单向的。可以看一下下面帖子对EMU0, EMU1管脚的作用。
https://e2echina.ti.com/support/processors/f/processors-forum/126332/jtag-emu0-emu1/353576
您的意思是做TRACE功能时,这两个脚是会发生从DSP对外输出的情况?
那么使用XDS100方式,不做TRACE功能时,这两个脚为什么连接FT232芯片的IO?这两个信号在调试和烧写是有规定的时序码?还是可以上拉接死,不用练IO?
请看下面的文档1.9.3 Using Emulation Pins 。
https://www.ti.com/lit/ug/spdu079a/spdu079a.pdf