This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: AM5728参考的IDK设计,但是启动后找不到phy地址

Part Number: AM5728


你好,

我们参考了5728 idk的设计,原理图设计的phy地址是0,但是使用idk的配置启动文件,找不到phy? 请帮忙看看是什么问题呢,谢谢。

[ 7.232331] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 7.287222] net eth1: initializing cpsw version 1.15 (0)
[ 7.287229] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[ 7.287233] cpsw 48484000.ethernet: ALE Table size 1024
[ 7.328762] libphy: PHY 48485000.mdio:01 not found
[ 7.328770] net eth1: phy "48485000.mdio:01" not found on slave 1, err -19
[ 7.343777] cpts ptp bc clkid 0
[ ! 7.381524] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 7.384610] net eth0: initializing cpsw version 1.15 (0)
[ 7.436152] libphy: PHY 48485000.mdio:00 not found
[ 7.436171] net eth0: phy "48485000.mdio:00" not found on slave 0, err -19
[ 7.454142] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ OK ] Started Network Service.

下面是完整的启动log
U-Boot 2017.01-gabc9806-dirty (Jan 12 2022 - 16:22:21 +0800)

@@@CPU : DRA752-GP ES2.0
Model: TI AM5728 IDK
Board: QuarkAnt
checkboard
DRAM: @@dram_init
2 GiB
@####board_init
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env

** Unable to read "uboot.env" from mmc0:1 **
Using default environment

@####setup_board_eeprom_env
@####invalid_eeprom
@####board_late_init
@####am57x_idk_lcd_detect
not detect boardtype
lcd dtect end
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: Could not get PHY for ethernet@484000: addr 0

Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3758320 bytes read in 1274 ms (2.8 MiB/s)
106344 bytes read in 48 ms (2.1 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe3000, end 8fffff67 ... OK

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.69 (wangp@wangp) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #1 SMP PREEMPT Thu Jan 13 10:37:25 CST 2022
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ ` 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt:Machine model: TI AM5728 IDK
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] OF: reserved mem: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] OF: reserved mem: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
[ 0.000000] OF: resevved mem: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000fe400000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000ffd00000 to fe600000 for dram barrier
[ 0.000000] DRA752 ES2.0
[ 0.000000] percpu: Embedded 13 pages/cpu @eed33000 s22028 r8192 d23028 u53248
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 471616
[ 0.000000] Kernel kommand line: console=ttyO2,115200n8 root=PARTUUID=000e9097-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1671600K/1893376K available (8192K kernel code, 317K rwdata, 2436K rodata, 2048K init, 304K bss, 33360K reserved, 188416K cma-reserved, 1278976K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0a00000 (10208 kB)
[ 0.000000] .init : 0xc0e00000 - 0xc1000000 (2048 kB)
[ 0.000000] .data : 0xc1000000 - 0xc104f408 ( 318 kB)
[ 0.000000] .bss : 0xc1051000 - 0xc109d170 ( 305 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000017] Switching to timer-based delay loop, resolution 162ns
[ 0.000324] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000332] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000757] Console: colour dummy device 80x30
[ 0.000773] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[ 0.000781] This ensures that you still see kernel messages. Please
[ 0.000787] update your kernel commandline.
[ 0.000803] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000817] pid_max: default: 32768 minimum: 301
[ 0.000920] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000931] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001547] CPU: Testing write buffer coherency: ok
[ 0.001754] /cpus/cpu@0 missing clock-frequency property
[ 0.001770] /cpus/cpu@1 missing clock-frequency property
[ 0.001781] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001798] Setting up static identity map for 0x80200000 - 0x80200060
[ 0.080059] EFI services will not be available.
[ 0.170264] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.170351] Brought up 2 CPUs
[ 0.170364] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.170372] CPU: All CPU(s) started in HYP mode.
[ 0.170378] CPU: Virtualization extensions available.
[ 0.170812] devtmpfs: initialized
[ 0.198834] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.199081] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.199097] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.202484] pinctrl core: initialized pinctrl subsystem
[ 0.203304] NET: Registered protocol family 16
[ 0.204166] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.205203] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.440365] cpuidle: using governor ladder
[ 0.470390] cpuidle: using governor menu
[ 0.480271] OMAP GPIO hardware version 0.1
[ 0.495087] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.520775] No ATAGs?
[ 0.520799] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.520809] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.521174] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.521184] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.521726] OMAP DMA hardware revision 0.0
[ 0.561602] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.562858] edma 43300000.edma: memcpy is disabled
[ 0.567594] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.571461] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.571643] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.571803] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.571958] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.572216] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.572406] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.575058] palmas 0-0058: Irq flag is 0x00000004
[ 0.602937] palmas 0-0058: Muxing GPIO 2b, PWM 0, LED 0
[ 0.606093] SMPS3: supplied by VMAIN
[ 0.609395] SMPS6: supplied by VMAIN
[ 0.611130] SMPS7: supplied by VMAIN
[ 0.613024] SMPS8: supplied by VMAIN
[ 0.614748] SMPS9: supplied by VMAIN
[ 0.615676] V3_3D: supplied by smps9
[ 0.615853] random: fast init done
[ 0.615902] vtt_fixed: supplied by V3_3D
[ 0.616004] LDO1: supplied by VMAIN
[ 0.621390] LDO2: supplied by VMAIN
[ 0.631238] LDO3: supplied by VMAIN
[ 0.641250] LDO4: supplied by VMAIN
[ 0.653347] LDO9: supplied by VMAIN
[ 0.661644] LDOLN: supplied by VMAIN
[ 0.671365] LDOUSB: supplied by VMAIN
[ 0.684447] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.684635] media: Linux media interface: v0.10
[ 0.684683] Linux video capture interface: v2.00
[ 0.684718] pps_core: LinuxPPS API ver. 1 registered
[ 0.684725] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.684745] PTP clock support registered
[ 0.684775] EDAC MC: Ver: 3.0.0
[ 0.685692] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[ 0.685992] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[ 0.686279] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.686563] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.686883] Advanced Linux Sound Architecture Driver Initialized.
[ 0.687682] clocksource: Switched to clocksource arch_sys_counter
[ 0.697922] NET: Registered protocol family 2
[ 0.698423] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.698486] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.698612] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.698656] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.698686] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.698862] NET: Registered protocol family 1
[ 0.699174] RPC: Registered named UNIX socket transport module.
[ 0.699184] RPC: Registered udp transport module.
[ 0.699191] RPC: Registered tcp transport module.
[ 0.699197] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.700102] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.703032] workingset: timestamp_bits=14 max_order=19 bucket_order=5
[ 0.710574] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.711312] NFS: Registering the id_resolver key type
[ 0.711334] Key type id_resolver registered
[ 0.711341] Key type id_legacy registered
[ 0.711379] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.712565] bounce: pool size: 64 pages
[ 0.712708] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 0.712718] io scheduler noop registered
[ 0.712726] io scheduler deadline registered
[ 0.712860] io scheduler cfq registered (default)
[ 0.718046] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.720661] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.3
[ 0.720979] OF: PCI: host bridge /ocp/axi@0/pcie@51000000 ranges:
[ 0.720990] OF: PCI: No bus range found for /ocp/axi@0/pcie@51000000, using [bus 00-ff]
[ 0.721023] OF: PCI: IO 0x20003000..0x20012fff -> 0x00000008
[ 0.721045] OF: PCI: MEM 0x20013000..0x2fffffff -> 0x20013000
[ 1.722442] dra7-pcie 51000000.pcie: phy link never came up
[ 1.722610] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 1.722623] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.722633] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 1.722644] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 1.723021] PCI: bus0: Fast back to back transfers disabled
[ 1.723134] PCI: bus1: Fast back to back transfers enabled
[ 1.723251] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 1.723267] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 1.723280] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 1.723508] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 1.784849] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 1.788226] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 301, base_baud = 3000000) is a 8250
[ 2.771256] console [ttyS2] enabled
[ 2.776592] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 2.783368] [drm] Initialized
[ 2.788126] OMAP DSS rev 6.1
[ 2.791455] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 2.799884] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
[ 2.870826] brd: module loaded
[ 2.899126] loop: module loaded
[ 2.906159] m25p80 spi0.0: unrecognized JEDEC id bytes: 00, 00, 00
[ 2.913036] libphy: Fixed MDIO Bus: probed
[ 2.977710] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 2.983832] davinci_mdio 48485000.mdio: no live phy, scanning all
[ 2.991071] davinci_mdio: probe of 48485000.mdio failed with error -5
[ 2.998163] cpsw 48484000.ethernet: Detected MACID = 00:35:ff:ad:68:42
[ 3.004776] cpsw 48484000.ethernet: device node lookup for pps timer failed
[ 3.011822] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
[ 3.019999] cpsw 48484000.ethernet: cpsw: Detected MACID = 00:35:ff:ad:68:43
[ 3.028565] mousedev: PS/2 mouse device common for all mice
[ 3.034478] i2c /dev entries driver
[ 3.044597] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 3.118037] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 3.124417] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 3.208744] ledtrig-cpu: registered to indicate activity on CPUs
[ 3.218776] NET: Registered protocol family 10
[ 3.233887] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.240246] NET: Registered protocol family 17
[ 3.244838] Key type dns_resolver registered
[ 3.249232] omap_voltage_late_init: Voltage driver support not added
[ 3.255678] Power Management for TI OMAP4+ devices.
[ 3.260796] Registering SWP/SWPB emulation handler
[ 3.274007] dmm 4e000000.dmm: workaround for errata i878 in use
[ 3.281231] dmm 4e000000.dmm: initialized all PAT entries
[ 3.287948] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.294591] [drm] No driver support for vblank timestamp query.
[ 3.300564] omapdrm omapdrm.0: No connectors reported connected with modes
[ 3.307470] [drm] Cannot find any crtc or sizes - going 1024x768
[ 3.316277] [drm] Enabling DMM ywrap scrolling
[ 3.325065] Console: switching to colour frame buffer device 128x48
[ 3.335058] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 3.378685] hctosys: unable to open rtc device (rtc0)
[ 3.384685] ALSA device list:
[ 3.387662] No soundcards found.
[ 3.391650] Waiting for root device PARTUUID=000e9097-02...
[ 3.416526] mmc0: host does not support reading read-only switch, assuming write-enable
[ 3.431863] mmc0: new ultra high speed SDR104 SDHC card at address aaaa
[ 3.438841] mmcblk0: mmc0:aaaa SC32G 29.7 GiB
[ 3.447263] mmcblk0: p1 p2
[ 3.491755] mmc1: new DDR MMC card at address 0001
[ 3.496854] mmcblk1: mmc1:0001 BJTD4R 29.1 GiB
[ 3.501554] mmcblk1boot0: mmc1:0001 BJTD4R partition 1 4.00 MiB
[ 3.507633] mmcblk1boot1: mmc1:0001 BJTD4R partition 2 4.00 MiB
[ 3.516426] mmcblk1: p1 p2
[ 3.658043] EXT4-fs (mmcblk0p2): recovery complete
[ 3.665932] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.674119] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 3.684419] devtmpfs: mounted
[ 3.688530] Freeing unused kernel memory: 2048K
[ 3.749157] omap_hsmmc 4809c000.mmc: ADMA err: ST_TFR, desc at 0xfe444010 follows the erroneous one
[ 3.836715] systemd[1]: System time before build time, advancing cloc
[ 3.862062] systemd[1]: systemd 230 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 3.880480] systemd[1]: Detected architecture arm.

Welcome to Arago 2017.12!

[ 3.920723] systemd[1]: Set hostname to <am57xx-evm>.
[ 4.177968] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 4.220909] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.247887] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.279667] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 4.309762] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.348617] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.378334] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ OK ] Created slice system-getty.slice.
[ OK ] Reached target Slices.
[ OK ] Reached target Remote File Systems.
Starting Create Static Device Nodes in /dev...
[ 4.530566] omap_hsmmc 4809c000.mmc: ADMA err: ST_TFR, desc at 0xfe444010 follows the erroneous one
Starting alignment.service...
[ OK ] Reached target Swap.
Starting Remount Root and Kernel File Systems...
[ 4.642024] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ OK ] Listening on Process Core Dump Socket.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
Starting Setup Virtual Console...
Mounting Temporary Directory...
[ OK ] Listening on Network Service Netlink Socket.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ OK ] Reached target Paths.
[ OK ] 蘨stening on udev Control Socket.
[ OK ] Listening on Syslog Socket.
Starting Journal Service...
[ OK ] Listening on udev Kernel Socket.
[ OK ] Mounted Debug File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Temporary Directory.
[ OK ] Started Journal Service.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Started alignment.service.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Setup Virtual Console.
Starting udev Coldplug all Devices...
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Mounting Configuration File System...
Starting Apply Kernel Variables...
Starting Flush Journal to Persistent Storage...
[ OK ] Mounted Configuration File System.
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Apply Kernel Variables.
[ 5.855202] systemd-journald[124]: Received request to flush runtime journal from PID 1
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Load/Save Random Seed.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
Starting Network Time Synchronization...
[ OK ] Started Updcte UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Found device /dev/ttyS2.
[ OK ] Reached target System Time Synchronized.
[ OK ] Reached target System Initialization.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started System Logging Service.
Starting uim-sysfs.service...
Starting Print notice about GPLv3 packages...
Starting Telephony service...
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Periodic Command Scheduler.
Starting TI MultiCore Tools Daemon...
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Telephony service.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
Starting Network Service...
[ OK ] Started Job spooling tools.
Starting Login Service...
[ OK ] Started Kernel Logging Service.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[FAILED] Failed to start TI MultiCore Tools Daemon.
See 'systemctl status ti-mct-daemon.service' for details.
[ 7.232331] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 7.287222] net eth1: initializing cpsw version 1.15 (0)
[ 7.287229] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[ 7.287233] cpsw 48484000.ethernet: ALE Table size 1024
[ 7.328762] libphy: PHY 48485000.mdio:01 not found
[ 7.328770] net eth1: phy "48485000.mdio:01" not found on slave 1, err -19
[ 7.343777] cpts ptp bc clkid 0
[ ! 7.381524] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 7.384610] net eth0: initializing cpsw version 1.15 (0)
[ 7.436152] libphy: PHY 48485000.mdio:00 not found
[ 7.436171] net eth0: phy "48485000.mdio:00" not found on slave 0, err -19
[ 7.454142] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ OK ] Started Network Service.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.