CCS 11: https://www.ti.com/tool/download/CCSTUDIO
XDS560Plus 驱动 : https://www.arrowsolution.com.cn/Public/Home/down/1441789634_1327592584.rar
verify 时会卡住

debug 时会卡在 configuring debugger 界面。

向任何回答表示感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CCS 11: https://www.ti.com/tool/download/CCSTUDIO
XDS560Plus 驱动 : https://www.arrowsolution.com.cn/Public/Home/down/1441789634_1327592584.rar
verify 时会卡住

debug 时会卡在 configuring debugger 界面。

向任何回答表示感谢!
target configuration file里选择的是TI的xds560仿真器,不是seed的xds560仿真器。如果安装正确的话,应该有seed的仿真器选项。可以看一下下面的seed仿真器安装使用手册。
https://www.arrowsolution.com.cn/Public/Home/down/1509948026_1040710363.pdf
这是安装完 SEEDXDS560 驱动后新增的文件:
├── common
│ ├── targetdb
│ │ └── connections
│ │ └── SEED-XDS560PLUS_Connection.xml
│ └── uscif
│ ├── uscif.out
│ ├── xds560.out
│ └── xds560v26.out
└── emulation
└── seed
├── SEED-XDS560PLUS Version.exe
├── seedxds560usb.inf
├── seedxds560usb.sys
├── seedxds560usb_ntamd64.cat
├── seedxds560usbv26.sys
└── USBorPCI.exe
6 directories, 10 files
我对比了一下 SEED-XDS560PLUS_Connection.xml TIXDS560_Connection.xml,发现
前者少了ID 为 DiagnosticCommand 的属性:
<property Name="Diagnostic Command" Type="hiddenfield" Value="%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity" ID="DiagnosticCommand"/>
从TIXDS560_Connection.xml复制这一行后,SEEDXDS560 的 verify connection 和test
connection不再是灰色的了,但还是会卡死,就跟之前选 TIXDS560 时一样。
Load 或 debug 会报错:
IcePick_C_0: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.6.0.00172)
您好!现在换了一个仿真器,是TI的XDS100V3, 现在test connection 没有问题,但新建一个工程烧录程序时会出现如下错误:
C64XP: File Loader: Verification failed: Values at address 0x80000800 do not match Please verify target memory and memory map.
C64XP: GEL: File: C:\Users\wzy\Desktop\x264\Debug\x264.out: a data verification error occurred, file load failed.
我看了一下工程中默认生成的cmd中有
DDR2: o = 0x80000000 l = 0x20000000 /* 512MB of external DDR */
然后所有的sections都分配到DDR2上了。
请问这是什么原因?是DDR2有问题吗?该如何解决呢?比如把sections分配到别的什么地方吗?