This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CPU frequency based on platform library

各位大牛:

                 在platform_test工程文件中,对于CPU的PLL设定采用缺省值,在实验过程中,console窗口打印CPU frequency,可以得到2000MHz,这比1.25GHZ高了不少啊。我知道可以对pllm, plld,pllpost,plldiv等进行设置来实现1GHz1.25GHZ等主频。主要的疑问点是:

                 evm66787的CPU最大能够实现的频率是多少呢? 为何platform_test中可以实现2000MHz的频率,这是否能够真实的实现,还是大于1.25GHz 的设置都会运行在1.25GHz,而不管CPU频率寄存器中的值?我们打印出的信息只是寄存器中的值,而并不能够代表CPU正在运行的主频?

  • 这个手册上说最高是1.25GHz,我觉得是能超频的,但具体能超到多少就不清楚了,但我估计2Ghz是很不靠谱的,小心把片子给毁了。

  • 您好:

    我想问一下,如何用pllm, plld,pllpost,plldiv等进行设置来实现1GHz1.25GHZ等主频啊,还有,我用的不是EVM开发板,是定制的一个板子,我的输入时钟和EVM不同,那么如何利用platform库中的platform_init()函数来配置pll,ddr啊?