Part Number: AM3354
大家好,我是一名新手,如果问题太简单,请原谅
我直接把USB0_VBUS接5V,把USB0_ID直接接gnd,接usb typeA插座。插座的5V管脚也直接接5V电源,不受USB0_DRVVBUS控制。插入U盘时,usb0无法识别设备。
我用的Linux系统,不用drvvbus控制vbus上电,而是直接给vbus供电5v,听说只需要修改软件中的一个模式配置就可以实现USB的识别,请问软件如何修改?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3354
大家好,我是一名新手,如果问题太简单,请原谅
我直接把USB0_VBUS接5V,把USB0_ID直接接gnd,接usb typeA插座。插座的5V管脚也直接接5V电源,不受USB0_DRVVBUS控制。插入U盘时,usb0无法识别设备。
我用的Linux系统,不用drvvbus控制vbus上电,而是直接给vbus供电5v,听说只需要修改软件中的一个模式配置就可以实现USB的识别,请问软件如何修改?谢谢
USB作Host的话,建议DRVVBUS接5v,请看下面文档里的说明。
USBx_DRVVBUS should be connected to the enable of the 5 V VBUS power source
https://www.ti.com/lit/an/sprabn2a/sprabn2a.pdf
如果没接的话,需要打个补丁,请参考下面的帖子。
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/829149/am3358-usb-host-without-drvvus/3067983
您好,我在tmdssk3358评估板上移植了ubuntu18.04,也遇到了usb无法使用的问题,请问您是怎么解决的?