This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前没有这个错,今天才出现的,不知道法生了什么。test connection 没有问题
C64XP: Error connecting to the target: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.6.0.00172)
找到了这个帖子:
但板子是俊竹科技设计的,没有reset开关。
向任何回答表示感谢!
c/ti/ccs1110/ccs/ccs_base/emulation/boards/evmdm6467/gel/davincihd1080p_arm.gel 里有boot_dsp_from_arm 的语句,我试着重新开了一个arm项目,在arm 926 上加载了 c/ti/ccs1110/ccs/ccs_base/emulation/boards/evmdm6467/gel/davincihd1080p_arm.gel, 显示了以下信息:
ARM926: GEL Output: DaVinci HD1080p ARM Startup Sequence ARM926: GEL Output: Disable IRQ/FIQ ARM926: GEL Output: Flush Cache ARM926: GEL Output: Disable MMU ARM926: GEL Output: Enable Instruction Cache. ARM926: GEL Output: Setup PinMux...ARM926: GEL Output: [Done] ARM926: GEL Output: Setup Power Modules (All on)...ARM926: GEL Output: [Done] ARM926: GEL Output: Setup PLL0ARM926: GEL: Error while executing OnTargetConnect(): Target failed to write 0x01C40900 at (*(pll_ctl)&=~(0x0001)) [davincihd1080p_arm.gel:572] at setup_pll_0(0, 29) [davincihd1080p_arm.gel:655] at Setup_Pll0_990_MHz_OscIn() [davincihd1080p_arm.gel:43] at OnTargetConnect() ARM926: Error: (Error -1060 @ 0x2E18) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.6.0.00172) ARM926: Error: (Error -1029 @ 0x2B5F) Invalid data read from ICECrusher register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.6.0.00172) ARM926: Unable to determine target status after 20 attempts ARM926: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
但之后回到dsp的那个项目debug还是报错:
C64XP: Error connecting to the target: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.6.0.00172)
是我操作的问题吗?只要在arm的那个项目里debug就可以运行 boot_dsp_from_arm 了对吧?
test connection 的结果是正常的,仿真器应该没有坏:
[Start: Texas Instruments XDS100v3 USB Debug Probe] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\wzy\AppData\Local\TEXASI~1\CCS\ ccs1110\0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100- or 510-class product. This utility will load the adapter 'jioserdesusbv3.dll'. The library build date was 'Dec 8 2021'. The library build time was '11:16:32'. The library package version is '9.6.0.00172'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '4' (0x00000004). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the FTDI FT2232 with USB interface. The link from controller to target is direct (without cable). The software is configured for FTDI FT2232 features. The controller cannot monitor the value on the EMU[0] pin. The controller cannot monitor the value on the EMU[1] pin. The controller cannot control the timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '0' (0x0000). -----[The log-file for the JTAG TCLK output generated from the PLL]---------- Test Size Coord MHz Flag Result Description ~~~~ ~~~~ ~~~~~~~ ~~~~~~~~ ~~~~ ~~~~~~~~~~~ ~~~~~~~~~~~~~~~~~~~ 1 64 - 01 00 500.0kHz O good value measure path length 2 64 + 00 00 1.000MHz [O] good value apply explicit tclk There is no hardware for measuring the JTAG TCLK frequency. In the scan-path tests: The test length was 2048 bits. The JTAG IR length was 6 bits. The JTAG DR length was 1 bits. The IR/DR scan-path tests used 2 frequencies. The IR/DR scan-path tests used 500.0kHz as the initial frequency. The IR/DR scan-path tests used 1.000MHz as the highest frequency. The IR/DR scan-path tests used 1.000MHz as the final frequency. -----[Measure the source and frequency of the final JTAG TCLKR input]-------- There is no hardware for measuring the JTAG TCLK frequency. -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 64 32-bit words. The test for the JTAG IR instruction path-length succeeded. The JTAG IR instruction path-length is 6 bits. The test for the JTAG DR bypass path-length succeeded. The JTAG DR bypass path-length is 1 bits. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG IR Integrity scan-test has succeeded. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG DR Integrity scan-test has succeeded. [End: Texas Instruments XDS100v3 USB Debug Probe]
重新开了一个arm 工程,load 了一个gel文件,现在debug时报错:
ARM926: GEL Output: DaVinci HD1080p ARM Startup Sequence ARM926: GEL Output: Disable IRQ/FIQ ARM926: GEL Output: Flush Cache ARM926: GEL Output: Disable MMU ARM926: GEL Output: Enable Instruction Cache. ARM926: GEL Output: Setup PinMux...ARM926: GEL Output: [Done] ARM926: GEL Output: Setup Power Modules (All on)...ARM926: GEL Output: [Done] ARM926: GEL Output: Setup PLL0ARM926: GEL: Error while executing OnTargetConnect(): Target failed to write 0x01C40938 at (*(pll_cmd)|=0x0001) [davincihd1080p_arm.gel:619] at setup_pll_0(0, 29) [davincihd1080p_arm.gel:655] at Setup_Pll0_990_MHz_OscIn() [davincihd1080p_arm.gel:43] at OnTargetConnect() ARM926: GEL Output: Disable VPSS ARM926: GEL Output: Disable IRQ/FIQ ARM926: GEL Output: Flush Cache ARM926: GEL Output: Disable MMU ARM926: GEL Output: Disable EDMA events ARM926: GEL Output: ARM926: GEL Output: Disable VPSS ARM926: GEL Output: Disable IRQ/FIQ ARM926: GEL Output: Flush Cache ARM926: GEL Output: Disable MMU ARM926: GEL Output: Disable EDMA events ARM926: GEL Output: ARM968_0: File Loader: Verification failed: Target failed to write 0x80000800 ARM968_0: GEL: File: C:\Users\wzy\Desktop\x264-arm\Debug\x264-arm.out: Load failed.
还是arm核没有连上的原因吗?请问有什么可能的解决办法吗?
是在gel文件里load .out文件了?之前成功的情况下,也是用了这个gel文件?
一般流程是在ccs里手动connect,然后手动load .out文件。
我是在这里加载gel文件的。
之前成功指的是什么?之前遇到的问题就是没有加载gel,无法把程序烧录到外部的DDR2 https://e2echina.ti.com/support/processors/f/processors-forum/217114/tms320dm6467t-c64xp-file-loader-verification-failed-values-at-address-0x80000800-do-not-match
load .out 是指debug吗?手动 connect 是指 test connection吗?
这个是TI EVM板的gel文件,您的板子硬件和TI的EVM板一样吗?如果不一样的话,需要根据您板子的硬件修改gel文件。建议您联系板子厂家,他们对板子的配置熟悉。