Other Parts Discussed in Thread: AM4378,
Dears,
We use gpmc interface to connect to fpga( use addr/data mux mode, and async read/write ), on am4378 ,we read/write data both ok, now we should change to am5728 platfrom, then porting the gpmc config from am437x to am5728(and changed some time sequence), now, i can read and write data ok on address from 0~ 0x50000 ,but from address 0x50000 , I can not write data success, it seems that i can not operate the high address from 0x50000 to other. please help to check this issue, thanks so much.
read 0x400044 test
# cat dump_motor3_reg | grep 0x40044
reg0x40044 :0x0
//write 0x400044 address as 0xf3 data
# echo 0x40044 0xf3 > fpga_reg
//read again, and can write 0xf3 success.
# cat dump_motor3_reg | grep 0x40044
reg0x40044 :0xf3
now test 0x5300a :
//read 0x5300a address:
# cat dump_motor1_reg | grep 5300a
reg0x5300a :0x0
//write 0x5300a as 0xf3 data:
# echo 0x5300a 0xf3 > fpga_reg
//read back, also data is 0, not write success.
# cat dump_motor1_reg | grep 5300a
reg0x5300a :0x0
but on am4378 platform , there is no this issue, every address can operat success.
the u-boot gpmc pin config below:
we use ad[0-15] a[1]-a[6] , 16 + 6 = 22 => 4M space
const struct pad_conf_entry core_padconf_array_essential_am572x_idk[] = {
{GPMC_AD0, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD1, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD2, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD3, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD4, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD5, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD6, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD7, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD8, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD9, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD10, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD11, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD12, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD13, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD14, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_AD15, (M0 | PIN_INPUT_PULLUP)}, /* gpmc_a0.vin4b_d0 */
{GPMC_A1, (M0 | PIN_OUTPUT_PULLDOWN)}, /* gpmc_a1.vin4b_d1 */
{GPMC_A2, (M0 | PIN_OUTPUT_PULLDOWN)}, /* gpmc_a2.vin4b_d2 */
{GPMC_A3, (M0 | PIN_OUTPUT_PULLDOWN)}, /* gpmc_a3.vin4b_d3 */
{GPMC_A4, (M0 | PIN_OUTPUT_PULLDOWN)}, /* gpmc_a4.vin4b_d4 */
{GPMC_A5, (M0 | PIN_OUTPUT_PULLDOWN)}, /* gpmc_a5.vin4b_d5 */
{GPMC_A6, (M0 | PIN_OUTPUT_PULLDOWN)}, /* gpmc_a6.vin4b_d6 */
{GPMC_CLK, (M0 | PIN_OUTPUT)}, /* gpmc_a6.vin4b_d6 */
{GPMC_CS0, (M0 | PIN_OUTPUT)}, /* gpmc_a6.vin4b_d6 */
{GPMC_ADVN_ALE, (M0 | PIN_OUTPUT_PULLUP)}, /* gpmc_a6.vin4b_d6 */
{GPMC_OEN_REN, (M0 | PIN_OUTPUT_PULLUP)}, /* gpmc_a6.vin4b_d6 */
{GPMC_WEN, (M0 | PIN_OUTPUT_PULLUP)}, /* gpmc_a6.vin4b_d6 */
...
}
kernel dts config:
&gpmc {
status = "okay";
ranges = <0 0 0x04000000 0x06000000>; /* mayi fpga on CS0 space. Min partition = 128MB */
fpga@0,0 {
compatible = "mayi,gpmc-fpga";
reg = <0 0 0x04000000>;
bank-width = <2>;
gpmc,mux-add-data = <2>; //mux addr;
gpmc,rd-cycle-ns = <70>;
gpmc,access-ns = <60>;
gpmc,cs-on-ns = <0>; //4
gpmc,cs-rd-off-ns = <68>;
gpmc,adv-on-ns = <0>; //8
gpmc,adv-rd-off-ns = <23>;
gpmc,oe-on-ns = <26>;
gpmc,oe-off-ns = <64>;
gpmc,wr-cycle-ns = <60>;
gpmc,wr-access-ns = <60>; //?
gpmc,wr-data-mux-bus-ns = <26>;
gpmc,cs-wr-off-ns = <68>;
gpmc,adv-wr-off-ns = <23>;
gpmc,we-on-ns = <24>;
gpmc,we-off-ns = <64>;
//gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <10>;
gpmc,cycle2cycle-samecsen = <10>;
gpmc,cycle2cycle-diffcsen = <0>;
gpmc,page-burst-access-ns = <10>;
#address-cells = <1>;
#size-cells = <1>;
};
};