This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Whether the Ethernet time synchronization function can be integrated in autosar in the future

Part Number: TDA4VM


hi:

now I use ti-processor-sdk-rtos-j721e-evm-xxx;

I want to run autosar on all r5 cores;

I want to use the Ethernet time synchronization function on autosar, but I found that there is no corresponding cpts operation interface in mcal in mcu_sw.

Is there any plan to integrate this function in the future? If integrated, which version will add the corresponding code to MCAL middle.


If it is not integrated, when I develop the driver, I need the relevant register address and which file in the autosar architecture will provide the register access security interface file.

thank you very much