hi:
now I use ti-processor-sdk-rtos-j721e-evm-xxx;
I want to run autosar on all r5 cores;
I want to use the Ethernet time synchronization function on autosar, but I found that there is no corresponding cpts operation interface in mcal in mcu_sw.
Is there any plan to integrate this function in the future? If integrated, which version will add the corresponding code to MCAL middle.

If it is not integrated, when I develop the driver, I need the relevant register address and which file in the autosar architecture will provide the register access security interface file.
thank you very much