Part Number: AM5728



SYS_EDMA_TPCC
DSP1_EDMA_TPCC
DSP2_EDMA_TPCC
DSP_EDMA_TPCC
其中,SYS_EDMA_TPCC是否可以被DSP使用?
DSP_EDMA_TPCC 和DSP1_EDMA_TPCC/DSP2_EDMA_TPCC 有什么区别?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SYS_EDMA_TPCC是否可以被DSP使用?
可以,SYS_EDMA可以被所有的核使用。
DSP_EDMA_TPCC 和DSP1_EDMA_TPCC/DSP2_EDMA_TPCC 有什么区别?
各个核私有的。
/* EDMA3 TPCC region. */
#define EDMA3_CC_REGION (1U)
/* EDMA3 Event queue number. */
#define EVT_QUEUE_NUM (0U)
uint32_t edma_address = CSL_DSP_DSP_EDMA_CC_REGS;
void uart_task(UArg a0, UArg a1)
{
/*Pad configuration and PRCM enable*/
padConfig_prcmEnable();
/*Configure the EDMA clock */
PlatformEDMAWkupDepEnable();
/* Do EDMA init Done once in the beginning of application */
EDMAsetRegion(EDMA3_CC_REGION);
EDMA3Init(edma_address, EVT_QUEUE_NUM); // SOC_EDMA_TPCC_BASE_VIRT CSL_DSP_DSP_EDMA_CC_REGS
...
}
//Table 16-6. Connection of The Device DREQs to The DMA_CROSSBAR Inputs
#define DMA_XBAR_INST_TX (49U)
#define DMA_XBAR_INST_RX (50U)
//Table 5-7. DSP2_EDMA Default Request Mapping
#define DMA_XBAR_INST_TX_SRC CSL_XBAR_INST_DMA_DSP2_DREQ_16
#define DMA_XBAR_INST_RX_SRC CSL_XBAR_INST_DMA_DSP2_DREQ_17
/*
** This function configures the DMA crossbar for UART TX and RX events.
*/
static void EdmaEvtConfigure(void)
{
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_DSP2_DMA, DMA_XBAR_INST_TX,
DMA_XBAR_INST_TX_SRC);
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_DSP2_DMA, DMA_XBAR_INST_RX,
DMA_XBAR_INST_RX_SRC);
}
typedef enum
{
CSL_XBAR_DMA_CPU_ID_SYSTEM_DMA,
CSL_XBAR_DMA_CPU_ID_EDMA,
CSL_XBAR_DMA_CPU_ID_DSP1_DMA,
CSL_XBAR_DMA_CPU_ID_DSP2_DMA
} CSL_XbarDmaCpuId;
问题1:DSP2的EDMA_TPCC访问 CSL_DSP_DSP_EDMA_CC_REGS ,若要触发UART1_TX 事件,使用CSL_xbarDmaConfigure()函数进行事件映射,
void CSL_xbarDmaConfigure(CSL_XbarDmaCpuId dmaRegType, Uint32 dmaCrossbarInputNo, Uint32 dmaDreqToMapTo);
其中第一个参数是配置 CSL_XBAR_DMA_CPU_ID_DSP2_DMA吗?
问题2:CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_DSP2_DMA, DMA_XBAR_INST_TX,
DMA_XBAR_INST_TX_SRC);
DMA事件映射后,DMA通道是否必须为 CSL_xbarDmaConfigure(...)的第三个参数 dmaDreqToMapTo ?
其中第一个参数是配置 CSL_XBAR_DMA_CPU_ID_DSP2_DMA吗?
typedef enum
{
CSL_XBAR_DMA_CPU_ID_SYSTEM_DMA,
CSL_XBAR_DMA_CPU_ID_EDMA,
CSL_XBAR_DMA_CPU_ID_DSP1_DMA,
CSL_XBAR_DMA_CPU_ID_DSP2_DMA
} CSL_XbarDmaCpuId;
DMA事件映射后,DMA通道是否必须为 CSL_xbarDmaConfigure(...)的第三个参数 dmaDreqToMapTo ?
映射事件需一致。
/**
* @file bsp_uart_edma.c
*
* @brief This file tests the UART driver APIs in EDMA mode.
*
*/
#include <stdio.h>
#include <string.h>
#include <stdint.h>
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Log.h>
#include <xdc/runtime/Diags.h>
/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/hal/Hwi.h>
/* TI-RTOS Header files */
#include <ti/drv/gpio/GPIO.h>
/* CSL Header files */
#include <ti/csl/csl_chip.h>
#include <ti/csl/arch/c66x/interrupt.h>
#include <ti/csl/example/utils/uart_console/inc/uartConfig.h>
#include <ti/csl/soc.h>
#include <ti/csl/hw_types.h>
#include <ti/csl/csl_uart.h>
#include <ti/csl/csl_edma.h>
#include <ti/csl/arch/csl_arch.h>
/* OSAL Header files */
#include <ti/osal/osal.h>
/* UART Header files */
#include <ti/drv/uart/UART.h>
#include <ti/drv/uart/UART_stdio.h>
#include <ti/drv/uart/src/UART_osal.h>
#include <ti/drv/uart/soc/UART_soc.h>
#include <ti/board/src/evmAM572x/include/evmam572x_pinmux.h>
/****************************************************************************/
/* INTERNAL MACROS */
/****************************************************************************/
/* EDMA3 Event queue number. */
#define EVT_QUEUE_NUM (0U)
/* EDMA3 TPCC region. */
#define EDMA3_CC_REGION (2U)
/* PaRAM Set number for Dummy Transfer. */
#define DUMMY_CH_NUM (5U)
/* EDMA3 interrupt number. */
/* EDMA3 error interrupt number. */
//说明:Table 17-4. DSP2_INTC Default Interrupt Mapping 查看默认映射关系
/*
#if (EDMA3_CC_REGION==3)
#define EDMA3_CC_XFER_COMPLETION_INT 20 //TPCC_INT3 - EDMA CC region3 interrupt
#define EDMA3_CC_XFER_ERROR_INT 27
#elif (EDMA3_CC_REGION==2)
#define EDMA3_CC_XFER_COMPLETION_INT 19 //TPCC_INT2 - EDMA CC region2 interrupt
#define EDMA3_CC_XFER_ERROR_INT 27
#elif (EDMA3_CC_REGION == 1)
#define EDMA3_CC_XFER_COMPLETION_INT 18 //TPCC_INT1 - EDMA CC region1 interrupt
#define EDMA3_CC_XFER_ERROR_INT 27
#elif (EDMA3_CC_REGION == 0)
#define EDMA3_CC_XFER_COMPLETION_INT 17 //TPCC_INT0 - EDMA CC region0 interrupt
#define EDMA3_CC_XFER_ERROR_INT 27
#endif
*/
/* EDMA3 interrupt number. */
#define EDMA3_CC_XFER_COMPLETION_INT (75U)
#define XBAR_INST_CC_XFER_COMPLETION (CSL_XBAR_INST_DSP2_IRQ_75)
#define XBAR_INTR_SOURCE_CC_XFER_COMPLETION (CSL_XBAR_EDMA_TPCC_IRQ_REGION1)
/* EDMA3 error interrupt number. */
#define EDMA3_CC_XFER_ERROR_INT (76U)
#define XBAR_INST_CC_XFER_ERROR (CSL_XBAR_INST_DSP2_IRQ_76)
#define XBAR_INTR_SOURCE_CC_XFER_ERROR (CSL_XBAR_EDMA_TPCC_IRQ_REGION1)
/* DSP2 EDMA3 transfer event number */
/******************* Transmit related definitions **************************/
/*
** Transmit DMA Threshold Value. This is set in TX_DMA_THRESHOLD register.
*/
#define TX_DMA_THRESHOLD (5U)
/*
** Transmit Trigger Space value. Use this if TX Trigger Level granularity
** is selected to be 1.
*/
#define TX_TRIGGER_SPACE_GRAN_1 (8U)
/* Number of bytes transmitted by EDMA per TX event sent by UART. */
#define TX_BYTES_PER_EVENT (8U)
/******************* Receive related definitions ***************************/
/* Receiver Buffer Size. */
#define RX_BUFFER_SIZE (50U)
/* Receive DMA Threshold Value. */
#define RX_DMA_THRESHOLD (8U)
/* Number of bytes to be received from the user. */
#define NUM_RX_BYTES (8)
/******************* DMA XBAR related definitions ***************************/
/* DMA XBAR Instance for UART1 Tx/RX. Refer TRM for DMA XBAR instance numbers.*/
/* Wrapper Definitions. */
#define EDMA3_UART_TX_CHA_NUM (16U)
#define EDMA3_UART_RX_CHA_NUM (49U)
//Table 16-6. Connection of The Device DREQs to The DMA_CROSSBAR Inputs
#define DMA_XBAR_INST_TX (49U)
#define DMA_XBAR_INST_RX (50U)
//Table 16-89. EDMA Default Request Mapping
//#define DMA_XBAR_INST_TX_SRC CSL_XBAR_INST_DMA_EDMA_DREQ_48
//#define DMA_XBAR_INST_RX_SRC CSL_XBAR_INST_DMA_EDMA_DREQ_49
//Table 5-7. DSP2_EDMA Default Request Mapping
#define DMA_XBAR_INST_TX_SRC CSL_XBAR_INST_DMA_DSP2_DREQ_16
#define DMA_XBAR_INST_RX_SRC CSL_XBAR_INST_DMA_DSP2_DREQ_17
// EDMA3 参数
#define MAX_ACNT 1
#define MAX_CCNT 1
/* OPT Field specific defines */
#define OPT_SYNCDIM_SHIFT (0x00000002u)
#define OPT_TCC_MASK (0x0003F000u)
#define OPT_TCC_SHIFT (0x0000000Cu)
#define OPT_ITCINTEN_SHIFT (0x00000015u)
#define OPT_TCINTEN_SHIFT (0x00000014u)
#define OPT_TCCMOD_SHIFT (0x0000000Bu)
#define UART_EDMA3CC_OPT_FIFO_WIDTH ((uint32_t)0xFFFFF8FFU)
/**< Set FIFO Width for edma transfer */
#define UART_EDMA3CC_OPT_DAM_CONST_MODE ((uint32_t)0x00000002U)
/**< Set DAM in Constant Addressing Mode */
#define UART_EDMA3CC_OPT_SAM_INCR_MODE ((uint32_t)0xFFFFFFFEU)
/**< Set SAM in Increment Mode */
/****************************************************************************/
/* GLOBAL VARIABLES */
/****************************************************************************/
static void(*cb_Fxn[EDMA3_NUM_TCC]) (uint32_t tcc);
unsigned char intent[] =
"The application echoes the characters that you type on the console.\r\n";
unsigned char welcome[] = "StarterWare UART DMA application.\r\n";
unsigned char enter[] = "Please Enter 08 bytes from keyboard.\r\n";
volatile uint32_t clBackFlag = 0;
unsigned char rxBuffer[RX_BUFFER_SIZE];
/*
** Transmit Trigger Space value. This is applicable only when UART FIFO mode
** is used. Refer to the comments of the API UARTFIFOConfig() to find the
** possible values of TX Trigger Space.
*/
uint32_t txTrigSpace = TX_TRIGGER_SPACE_GRAN_1;
/*
** Number of bytes transmitted by EDMA per TX event sent by UART.
** In UART FIFO mode, this should be equal to the TX Trigger Space value.
*/
uint32_t txBytesPerEvent = TX_BYTES_PER_EVENT;
/*
** Receive DMA Thresold Level. This applies to both UART FIFO and Non-FIFO
** modes of operation. For FIFO mode, refer to the comments of the API
** UARTFIFOConfig() to find the possible values of RX Trigger Level.
** For Non-FIFO mode, this value is 1.
*/
uint32_t rxTrigLevel = RX_DMA_THRESHOLD;
/* Transmit DMA Threshold Level. This is set in TX_DMA_THRESHOLD register. */
uint32_t txThreshLevel = TX_DMA_THRESHOLD;
uint32_t uartBaseAddr = SOC_UART1_BASE;
uint32_t edma_address = CSL_DSP_DSP_EDMA_CC_REGS; //CSL_DSP_DSP_EDMA_CC_REGS CSL_DSP_EDMA_CC_REGS CSL_DSP_DSP2_EDMA_CC_REGS SOC_EDMA_TPCC_BASE_VIRT
//#pragma DATA_ALIGN (local_arr, 32) //256位地址对齐,地址的低5位为0
static uint8_t local_arr[256] = {0x55, 0x55, 0x55, 0x55, 0x55, 0x55, 0x55, 0x55, 0x11, 0x22, 0x33, 0x44, 0x66, 0xFF, 0xEE, 0xAA};
/****************************************************************************/
/* LOCAL FUNCTION DEFINITIONS */
/****************************************************************************/
static void edma_hwi_init(void);
static void Edma3CompletionIsr(void);
static void padConfig_prcmEnable()
{
uint32_t regVal = 0;
/* uart1 pinmux initialization */
CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_UART1_RXD_UART1_RXD_MUXMODE, 0x0U); //0x0: uart1_rxd
CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_UART1_RXD_UART1_RXD_SLEWCONTROL, 0x1U); //0x1: Slow slew is selected
CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_UART1_RXD_UART1_RXD_INPUTENABLE, 0x1U); //0x1: Receive mode is enabled
((CSL_padRegsOvly) CSL_MPU_CORE_PAD_IO_REGISTERS_REGS)->PAD_UART1_RXD = regVal; /* uart1_rxd.uart1_rxd */
CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_UART1_TXD_UART1_TXD_MUXMODE, 0x0U);
CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_UART1_TXD_UART1_TXD_SLEWCONTROL, 0x1U);
CSL_FINS(regVal, CONTROL_CORE_PAD_IO_PAD_UART1_TXD_UART1_TXD_INPUTENABLE, 0x1U);
((CSL_padRegsOvly) CSL_MPU_CORE_PAD_IO_REGISTERS_REGS)->PAD_UART1_TXD = regVal; /* uart1_txd.uart1_txd */
}
static void PlatformEDMAWkupDepEnable(void)
{
HW_WR_REG32(SOC_CORE_CM_CORE_BASE + PM_L3MAIN1_TPTC1_WKDEP, 0x1); //0x4a008700U + 0x78U = 0x4A00 8778U, CM_L3MAIN1_TPTC1_CLKCTRL
while ((HW_RD_REG32(SOC_CORE_CM_CORE_BASE +
PM_L3MAIN1_TPTC1_WKDEP) & 0x00030000U) != 0x0)
{
;
}
HW_WR_REG32(SOC_CORE_CM_CORE_BASE + PM_L3MAIN1_TPTC2_WKDEP, 0x1); //0x4A00 8780U,CM_L3MAIN1_TPTC2_CLKCTRL
while ((HW_RD_REG32(SOC_CORE_CM_CORE_BASE +
PM_L3MAIN1_TPTC2_WKDEP) & 0x00030000U) != 0x0)
{
;
}
HW_WR_REG32(SOC_CORE_CM_CORE_BASE + PM_L3MAIN1_TPCC_WKDEP, 0x1); //0x4A00 8770U,CM_L3MAIN1_TPCC_CLKCTRL
while ((HW_RD_REG32(SOC_CORE_CM_CORE_BASE +
PM_L3MAIN1_TPCC_WKDEP) & 0x00030000U) != 0x0)
{
;
}
}
/*
** This function configures the AINTC to receive EDMA3 interrupts.
*/
static void Edma3INTCConfigure(void)
{
//中断映射 -> 默认映射,无需重新映射
// CSL_xbarIrqConfigure(CSL_XBAR_IRQ_CPU_ID_DSP2,
// XBAR_INST_CC_XFER_COMPLETION,
// XBAR_INTR_SOURCE_CC_XFER_COMPLETION);
// CSL_xbarIrqConfigure(CSL_XBAR_IRQ_CPU_ID_DSP2,
// XBAR_INST_CC_XFER_ERROR,
// XBAR_INTR_SOURCE_CC_XFER_ERROR);
edma_hwi_init();
}
/*
** A wrapper function performing FIFO configurations.
*/
static void UartFIFOConfigure(void)
{
uint32_t fifoConfig = 0;
#if 0
/*
** Transmitter Trigger Level Granularity is 1.
** Receiver Trigger Level Granularity is 1.
** Transmit Trigger Space set 1.
** Receive Trigger level set 1.
** Clear the Trasnmit FIFO.
** Clear the Receive FIFO.
** DMA Mode enabling shall happen through SCR register.
** DMA Mode 1 is enabled.
*/
fifoConfig = UART_FIFO_CONFIG(UART_TRIG_LVL_GRANULARITY_1,
UART_TRIG_LVL_GRANULARITY_1,
1,
1,
1,
1,
UART_DMA_EN_PATH_SCR,
UART_DMA_MODE_3_ENABLE);
#else
/*
** Transmitter Trigger Level Granularity is 1.
** Receiver Trigger Level Granularity is 1.
** Transmit Trigger Space set using 'txTrigSpace'.
** Receive Trigger level set using 'rxTrigLevel'.
** Clear the Trasnmit FIFO.
** Clear the Receive FIFO.
** DMA Mode enabling shall happen through SCR register.
** DMA Mode 1 is enabled.
*/
fifoConfig = UART_FIFO_CONFIG(UART_TRIG_LVL_GRANULARITY_1,
UART_TRIG_LVL_GRANULARITY_1,
txTrigSpace, //8
rxTrigLevel, //8
1,
1,
UART_DMA_EN_PATH_SCR,
UART_DMA_MODE_3_ENABLE);
#endif
/* Configuring the FIFO settings. */
fifoConfig = UARTFIFOConfig(uartBaseAddr, fifoConfig);
Log_print1(Diags_ENTRY, "FCR: 0x%02x", fifoConfig);
}
/*
** A wrapper function performing Baud Rate settings.
*/
static void UartBaudRateSet(void)
{
uint32_t divisorValue = 0;
/* Computing the Divisor Value. */
divisorValue = UARTDivisorValCompute(UART_MODULE_INPUT_CLK,
BAUD_RATE_115200,
UART16x_OPER_MODE,
UART_MIR_OVERSAMPLING_RATE_42);
/* Programming the Divisor Latches. */
UARTDivisorLatchWrite(uartBaseAddr, divisorValue);
}
/*
** This function initializes the UART instance for use.
*/
static void UartInitialize(void)
{
/* Performing a module reset. */
//UARTModuleReset(uartBaseAddr);
/* Performing FIFO configurations. */
UartFIFOConfigure();
/* Selecting the method of setting the Transmit DMA Threshold value. */
UARTTxDMAThresholdControl(uartBaseAddr, UART_TX_DMA_THRESHOLD_REG);
/* Configuring the Transmit DMA Threshold value. */
UARTTxDMAThresholdValConfig(uartBaseAddr, txThreshLevel); //txThreshLevel = 5
/* Performing Baud Rate settings. */
UartBaudRateSet();
/* Switching to Configuration Mode B. */
UARTRegConfigModeEnable(uartBaseAddr, UART_REG_CONFIG_MODE_B);
/* Programming the Line Characteristics. */
UARTLineCharacConfig(uartBaseAddr,
(UART_FRAME_WORD_LENGTH_8 | UART_FRAME_NUM_STB_1),
UART_PARITY_NONE);
/* Disabling write access to Divisor Latches. */
UARTDivisorLatchDisable(uartBaseAddr);
/* Disabling Break Control. */
UARTBreakCtl(uartBaseAddr, UART_BREAK_COND_DISABLE);
/* Switching to UART16x operating mode. */
UARTOperatingModeSelect(uartBaseAddr, UART16x_OPER_MODE);
}
/*
** This function configures the DMA crossbar for UART TX and RX events.
*/
static void EdmaEvtConfigure(void)
{
CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_DSP2_DMA, DMA_XBAR_INST_TX, //??
DMA_XBAR_INST_TX_SRC);
// CSL_xbarDmaConfigure(CSL_XBAR_DMA_CPU_ID_DSP2_DMA, DMA_XBAR_INST_RX,
// DMA_XBAR_INST_RX_SRC);
}
/****************************************************************************/
/* */
/* 发送数据 */
/* */
/****************************************************************************/
void UartTransmitData(unsigned int tccNum, unsigned int chNum,
volatile char *buffer, unsigned int buffLength)
{
EDMA3CCPaRAMEntry paramSet;
unsigned char *p = (unsigned char *)¶mSet;
unsigned int icyc = 0;
/* Clean-up the contents of structure variable. */
for (icyc = 0; icyc < sizeof(paramSet); icyc++)
{
p[icyc] = 0;
}
// 配置参数 RAM
paramSet.srcAddr = (unsigned int)buffer;
// 接收缓存寄存器 / 发送保持寄存器 地址
paramSet.destAddr = uartBaseAddr + 0;
paramSet.aCnt = 1;
paramSet.bCnt = (unsigned short)buffLength;
paramSet.cCnt = 1;
// 源索引自增系数 1 即一个字节
paramSet.srcBIdx = (short)1u;
// 目标索引自增系数
paramSet.destBIdx = (short)0u;
// AB同步传输模式
paramSet.srcCIdx = (short)0u;
paramSet.destCIdx = (short)0u;
paramSet.linkAddr = (unsigned short)0xFFFFu;
paramSet.bCntReload = (unsigned short)0u;
/* OPT PaRAM entries. */
paramSet.opt = (uint32_t) 0x0;
/* Src is in INCR mode & Dest is in FIFO modes */
paramSet.opt &= UART_EDMA3CC_OPT_SAM_INCR_MODE; //[0]
paramSet.opt |= UART_EDMA3CC_OPT_DAM_CONST_MODE; //[1]
/* FIFO width is 8 bit */
//paramSet.opt &= UART_EDMA3CC_OPT_FIFO_WIDTH; //[10:8]
paramSet.opt &= ((uint32_t)0xFFFFFCFFU);
/* AB Synchronized Transfer. */
paramSet.opt |= (1 << EDMA_TPCC_OPT_SYNCDIM_SHIFT);
/* Setting the Transfer Complete Code(TCC). */
paramSet.opt |=
((tccNum << EDMA_TPCC_OPT_TCC_SHIFT) & EDMA_TPCC_OPT_TCC_MASK); //[17:12]
/* Enabling the Completion Interrupt. */
paramSet.opt |= (1 << EDMA_TPCC_OPT_TCINTEN_SHIFT); //[20]
Log_print2(Diags_ENTRY, "opt = 0x%02x, bCnt = 0x%02x", paramSet.opt, paramSet.bCnt); //0x110006
// 写参数 RAM
EDMA3SetPaRAM(edma_address, chNum, ¶mSet);
}
/*
** This function is used as a callback from EDMA3 Completion Handler.
*/
static void callback(uint32_t tccNum)
{
/* Disabling DMA Mode of operation in UART. */
UARTDMADisable(uartBaseAddr);
/* Disabling DMA transfer on the specified channel. */
EDMA3DisableTransfer(edma_address, tccNum, EDMA3_TRIG_MODE_EVENT);
clBackFlag = 1;
}
/*
** EDMA Completion Interrupt Service Routine(ISR).
*/
static void Edma3CompletionIsr(void)
{
volatile uint32_t pendingIrqs;
uint32_t index = 1;
uint32_t count = 0;
if (EDMA3GetIntrStatus(edma_address))
{
/*
** Wait for a finite time to monitor the EDMA Completion Interrupt
** status.
*/
while ((count < EDMA3CC_COMPL_HANDLER_RETRY_COUNT) && (index != 0U))
{
index = 0;
/* Get the Interrupt status. */
pendingIrqs = EDMA3GetIntrStatus(edma_address);
while (pendingIrqs)
{
if ((pendingIrqs & 1U) == TRUE)
{
/* Clear the interrupt status. */
EDMA3ClrIntr(edma_address, index);
(*cb_Fxn[index])(index);
}
++index;
pendingIrqs >>= 1U;
}
count++;
}
}
#if 0
if(EDMA3IntrStatusHighGet(edma_address))
{
Log_print1(Diags_ENTRY, "------------------> EDMA3IntrStatusHighGet: 0x%02x", EDMA3IntrStatusHighGet(edma_address));
while ((count < EDMA3CC_COMPL_HANDLER_RETRY_COUNT) && (index != 0U))
{
index = 32;
pendingIrqs = EDMA3IntrStatusHighGet(edma_address);
while(pendingIrqs)
{
if( (pendingIrqs & 1U) == TRUE )
{
EDMA3ClrIntr(edma_address, index);
if(cb_Fxn[index])
{
(*cb_Fxn[index])(index);
}
}
}
}
}
#endif
}
/*
** EDMA Error Interrupt Service Routine(ISR).
*/
static void Edma3ErrorIsr(void)
{
volatile uint32_t pendingIrqs = 0;
uint32_t evtqueNum = 0;
uint32_t index = 1;
uint32_t Cnt = 0;
Log_print2(Diags_ENTRY, "EDMA3GetErrIntrStatus: 0x%02x, EDMA3GetCCErrStatus: 0x%02x", EDMA3GetErrIntrStatus(edma_address), EDMA3GetCCErrStatus(edma_address));
Log_print1(Diags_ENTRY, "EDMA3ErrIntrHighStatusGet: 0x%02x", EDMA3ErrIntrHighStatusGet(edma_address));
if ((0 != EDMA3GetErrIntrStatus(edma_address)) ||
(0 != (EDMA3GetCCErrStatus(edma_address))))
{
/* Loop for EDMA3CC_ERR_HANDLER_RETRY_COUNT number of time, breaks
* when no pending interrupt is found */
while ((Cnt < EDMA3CC_ERR_HANDLER_RETRY_COUNT) && (index != 0U))
{
index = 0U;
pendingIrqs = EDMA3GetErrIntrStatus(edma_address);
while (pendingIrqs)
{
/*Process all the pending interrupts*/
if ((pendingIrqs & 1U) == TRUE)
{
/* Writing to EMCR to clear the corresponding EMR bits.
* Also clearing any Secondary events in SER. */
EDMA3ClrMissEvt(edma_address, index);
}
++index;
pendingIrqs >>= 1U;
}
index = 0U;
pendingIrqs = EDMA3GetCCErrStatus(edma_address);
if (pendingIrqs != 0U)
{
/* Process all the pending CC error interrupts. */
/* Queue threshold error for different event queues. */
for (evtqueNum = 0U; evtqueNum < EDMA3_0_NUM_EVTQUE;
evtqueNum++)
{
if ((pendingIrqs & (1U << evtqueNum)) != 0U)
{
/* Clear the error interrupt. */
EDMA3ClrCCErr(edma_address, (1U << evtqueNum));
}
}
/* Transfer completion code error. */
if ((pendingIrqs & (1 << EDMA_TPCC_CCERR_TCERR_SHIFT)) != 0U)
{
EDMA3ClrCCErr(edma_address,
(0x01U << EDMA_TPCC_CCERR_TCERR_SHIFT));
}
++index;
}
Cnt++;
}
}
Log_print2(Diags_ENTRY, "EDMA3GetErrIntrStatus: 0x%02x, EDMA3GetCCErrStatus: 0x%02x", EDMA3GetErrIntrStatus(edma_address), EDMA3GetCCErrStatus(edma_address));
Log_print1(Diags_ENTRY, "EDMA3ErrIntrHighStatusGet: 0x%02x", EDMA3ErrIntrHighStatusGet(edma_address));
}
#define DSP1_EDMA3_CC_XFER_COMPLETION_INT 19 //TPCC_INT2 - EDMA CC region2 interrupt
#define DSP1_EDMA3_CC_ERROR_INT 27
static void edma_cb_isr(UInt32 event_id)
{
switch(event_id) {
case DSP1_EDMA3_CC_XFER_COMPLETION_INT: /* Transfer completed successfully */
Edma3CompletionIsr();
break;
case DSP1_EDMA3_CC_ERROR_INT: /* Transfer resulted in error. */
Edma3ErrorIsr();
break;
default:
break;
};
}
static void edma_hwi_init(void)
{
Hwi_Params hwiParams;
Error_Block eb;
Hwi_Params_init(&hwiParams);
Error_init(&eb);
/* set the event id of the peripheral assigned to this interrupt */
hwiParams.eventId = DSP1_EDMA3_CC_XFER_COMPLETION_INT;
/* set the argument passed to ISR function */
hwiParams.arg = DSP1_EDMA3_CC_XFER_COMPLETION_INT;
hwiParams.maskSetting = Hwi_MaskingOption_SELF;
Hwi_create(11, edma_cb_isr, &hwiParams, &eb);
if (Error_check(&eb)) {
Log_print0(Diags_INFO, "Hwi create failed \n");
return ;
}
/* set the event id of the peripheral assigned to this interrupt */
hwiParams.eventId = DSP1_EDMA3_CC_ERROR_INT;
/* set the argument passed to ISR function */
hwiParams.arg = DSP1_EDMA3_CC_ERROR_INT;
hwiParams.maskSetting = Hwi_MaskingOption_SELF;
Hwi_create(12, edma_cb_isr, &hwiParams, &eb);
if (Error_check(&eb)) {
Log_print0(Diags_INFO, "Hwi create failed \n");
return ;
}
// Hwi_enable();
}
void uart_task(UArg a0, UArg a1)
{
uint32_t icyc = 0;
for(icyc=0; icyc<256; icyc++)
{
local_arr[icyc] = icyc+1;
}
Log_print0(Diags_ENTRY, "uart_task | edma | 20220401-V5.3.1");
/*Pad configuration and PRCM enable*/
padConfig_prcmEnable();
/*Configure the EDMA clock */
PlatformEDMAWkupDepEnable();
/* Do EDMA init Done once in the beginning of application */
EDMAsetRegion(EDMA3_CC_REGION);
EDMA3Init(edma_address, EVT_QUEUE_NUM); // SOC_EDMA_TPCC_BASE_VIRT CSL_DSP_DSP_EDMA_CC_REGS
Edma3INTCConfigure();
UartInitialize();
EdmaEvtConfigure();
/* Request DMA Channel and TCC for UART Transmit*/
EDMA3RequestChannel(edma_address, EDMA3_CHANNEL_TYPE_DMA,
EDMA3_UART_TX_CHA_NUM, EDMA3_UART_TX_CHA_NUM,
EVT_QUEUE_NUM);
/* Registering Callback Function for TX*/
cb_Fxn[EDMA3_UART_TX_CHA_NUM] = &callback;
icyc = 8;
/* Configuring EDMA PaRAM sets to transmit 'welcome' message. */
UartTransmitData(EDMA3_UART_TX_CHA_NUM,
EDMA3_UART_TX_CHA_NUM,
(volatile char *)local_arr,
icyc++);
// 使能 EDMA3 通道
EDMA3EnableTransfer(edma_address, EDMA3_UART_TX_CHA_NUM, EDMA3_TRIG_MODE_EVENT); //EDMA3_TRIG_MODE_EVENT EDMA3_TRIG_MODE_MANUAL
/* Enabling DMA Mode 3. */
UARTDMAEnable(uartBaseAddr, UART_DMA_MODE_3_ENABLE);
while(1)
{
if(clBackFlag == 1)
{
clBackFlag = 0;
/* Configuring EDMA PaRAM sets to transmit 'welcome' message. */
UartTransmitData(EDMA3_UART_TX_CHA_NUM,
EDMA3_UART_TX_CHA_NUM,
(volatile char *)local_arr,
icyc);
// 使能 EDMA3 通道
EDMA3EnableTransfer(edma_address, EDMA3_UART_TX_CHA_NUM, EDMA3_TRIG_MODE_EVENT); //EDMA3_TRIG_MODE_EVENT EDMA3_TRIG_MODE_MANUAL
/* Enabling DMA Mode 3. */
UARTDMAEnable(uartBaseAddr, UART_DMA_MODE_3_ENABLE);
icyc++;
if(icyc == 70)
{
icyc = 0;
break;
}
}
Task_sleep(100);
}
/******************* Freeing of allocated channels **********************/
/* Free EDMA3 Channels for TX and RX */
// EDMA3FreeChannel(edma_address, EDMA3_CHANNEL_TYPE_DMA,
// EDMA3_UART_TX_CHA_NUM, EDMA3_TRIG_MODE_MANUAL,
// EDMA3_UART_TX_CHA_NUM, EVT_QUEUE_NUM);
}

目前,我已实现UART EDMA发送数据,但是存在BUG,只能发送8-65字节的数据,若发送数据长度小于8字节,则无法发送数据,发送数据长度大于65字节,则只能发送65字节,超出部分的数据丢失。能帮我看下我的配置哪里出问题吗?
我怀疑是UART FIFO配置异常,还有就是,PaRAM参数的opt[DAM],应该设置为INCR还是FIFO,若设置为FIFO,则FWID应该设置为多少?
跟这个帖子中的现象有点像,参考以下帖子的讨论看一下,可能是FIFO下EDMA配置的问题。
https://e2echina.ti.com/support/processors/f/processors-forum/190473/c6678-dma/586483