This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138: OMAP-L138_FlashAndBootUtils_2_40实现SPI烧写

Part Number: OMAP-L138


各位工程师你们好,

          目前我需要用SPI将bin文件烧写到flash里面,我采用的是SPI1,但目前我遇到一个奇怪的问题,我的CS信号一直没法拉低,片选不上,请问这个配置需要在哪里配置,目前我的配置如下:device_spi.h

PINmux采用4pin模式,PINMUX和PSC的配置如下:

我用示波器测试CS管脚一直为高