This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138: SPI_FLASH历程的使用和flash双备份

Part Number: OMAP-L138


工程师们,
       你们好!
       目前我在使用贵公司omapl138板卡时遇到以下问题:
       1、目前我将omapl138板卡的SPI1接到了一片flash(W25Q64JVZEIQ)上,使用贵司提供的..\OMAPL138\Demo\StarterWare\Application目录下的SPI_FLASH历程进行程序烧写,但在调试过程中发现,该历程在擦写Flash过不了,程序一直在进行忙检测
   statusGet()函数执行后rx_data[1]位置上的值一直为0xff,while过不去,用示波器查看 W25Q64JVZEIQ芯片的CS管脚(1管脚)发现一直为高电平,输入的时钟为20.8MHz,目前程序是配置为SPI_MASTER,查看SPI的寄存器状态并参考OMAP-L138 Technical Reference Manual文档发现,SPI初始化的过程已经完成,并且寄存器的状态的配置没有出错,但还是无法成功烧写,请问下这个问题该如何解决?期待您的回复。
     2、目前想在omapl138的nandflash部分进行烧写双备份的开发,即flash中存放两个固件,采用一定的机制(这个机制自定义)选择引导哪个版本的固件起来(目前我们是用omapl-138跑sys/bios)
首先想问omapl138板卡的bootloder程序用户可更改吗,请问关于该功能的开发,有可参考的文档或者案例吗?
    如能收到您的回复,不胜感激!