各位大侠:
小弟dm8127相机在系统启动时出现以下问题:
系统启动:
B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H
.@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.
.A@@#5r;;;r;;;rrr;r:r#AsM@@H.
;&@@@@MhXS5i5SX9B@@@@G;
:ihM#@@@@@##hs,
I2C read: I/O error
Error reading tps65911.
## Get date failed
Net: <ethaddr> not set. Reading from E-fuse
Detected MACID:40:5f:c2:26:5:a1
cpsw
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
** Can't read from device 0 **
** Unable to use mmc 0:1 for fatload **
In case ENV on MMC/SD is required
Please put a valid script named boot.scr on the card
Refer to the User Guide on how to generate the image
TI8148_IPNC#
网络烧写kernel时,设置tftp server参数:
TI8148_IPNC#setenv serverip 192.168.8.121
TI8148_IPNC#save
Saving Environment to NAND...
Erasing Nand...
Warning: Erase size 0x00002000 smaller than one erase block 0x00020000
Erasing 0x00020000 instead
阻塞到这里不动;
请问怎么解决啊?谢谢了!!!