This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8127参考样机系统启动问题

Other Parts Discussed in Thread: TPS65911

各位大侠:

小弟dm8127相机在系统启动时出现以下问题:

系统启动:  

    B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H     
              .@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@.      
                .A@@#5r;;;r;;;rrr;r:r#AsM@@H.        
                   ;&@@@@MhXS5i5SX9B@@@@G;           
                       :ihM#@@@@@##hs,               

I2C read: I/O error
Error reading tps65911.
## Get date failed
Net:   <ethaddr> not set. Reading from E-fuse
Detected MACID:40:5f:c2:26:5:a1
cpsw
Hit any key to stop autoboot:  0
Card did not respond to voltage select!
** Can't read from device 0 **

** Unable to use mmc 0:1 for fatload **
In case ENV on MMC/SD is required
Please put a valid script named boot.scr on the card
Refer to the User Guide on how to generate the image
TI8148_IPNC#


网络烧写kernel时,设置tftp server参数:

TI8148_IPNC#setenv serverip 192.168.8.121
TI8148_IPNC#save
Saving Environment to NAND...
Erasing Nand...
Warning: Erase size 0x00002000 smaller than one erase block 0x00020000
         Erasing 0x00020000 instead
阻塞到这里不动;

 

请问怎么解决啊?谢谢了!!!