This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于MCFW(DM8168)的采集信号的分辨率的切换



各位好!我现在采用的是DM8168的硬件平台,软件开发环境为DVRRDK_03.50.00.05.现在遇到的问题如下:

1、我的chains为CAP->DIS,为什么对于隔行扫描的输入信号(1080I_50/PAL/NTSC)显示出来的图像只有一场的数据?与此相似,我曾经搭建过这样的chains:CAP->NSF->MERGE->ENC,编码之后出来的数据也是只有一场的数据。不知为什么?

2、我想做各个分辨率之间的自动切换,如我接了1080I_60的信源,然后再切换到PAL的信源之上,有一种方案是删除chains中的所有link,然后再重新建立chains。这种方案执行之后,针对隔行扫描的信源会出现上下两场数据,上场的数据稳定,下场一直在闪烁。不知道为什么?各个分辨率之间的切换,除了此种方案还有哪些方案呢?

3、我想将各个LINK之后的数据采集、存储下来,看看是什么样的格式。但是不知应该怎样将数据由各个lINK传输到应用层呢?

非常感谢各位关注!!!!!!!

  • 你好,

     1、我的chains为CAP->DIS,为什么对于隔行扫描的输入信号(1080I_50/PAL/NTSC)显示出来的图像只有一场的数据?与此相似,我曾经搭建过这样的chains:CAP->NSF->MERGE->ENC,编码之后出来的数据也是只有一场的数据。不知为什么?

      在CAP之后需要经过DEI模块,这时候DEI输出的图像就是一帧的图像,可以用来显示,然后金果NSF之后进行编码。

     

  • 谢谢您的回复!!!按照您的指点,我又重新更新了chains:CAP->NSF->DEI->MERGE->ENC,按照这样在信源分辨率为1080I_60的时候,可以看到一帧的画面。但是针对1080I_50和PAL的信源,则发现只有一场的数据,而且编码之后的数据居然也是1080I_60。不知问题在哪?能否指点一二?
    非常感谢!!!!!
  • 补充一下:在信源分辨率为PAL和1080I_50的时候,编码出来的图像是整幅图像分为上下两部,上半部为正常图像,下半部为灰色。

    期待您的解答!!!!非常感谢!!!!!

  • 检查一下你的DEI的参数配置,对于1080I50与1080I60的参数是不同的。