This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 寄存器写出现错误 Debug 时出现程序加载错误 Trouble Writing Memory Block at 0x8ec600 on Page 0 of Length 0x7cc0



各位大神,我有以下问题请教,希望百忙中抽点时间回答,谢谢!
当FFT点数为32K浮点复数时会出现如下问题(FFT点数为4K,8K和16K时没有出现):
数据存在.DDR3段,
DDR3定义为:
DDR3:org 0x80000000 len=0x10000000
.DDR3:load >>DDR3
C66xx_0: Trouble Writing Memory Block at 0x8ec600 on Page 0 of Length 0x7cc0: (Error -1190 @ 0x8EC600) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0) 
C66xx_0: GEL: File: F:\13516test\DSPF_sp_fftSPxSP_66_LE_ELF\Debug\DSPF_sp_fftSPxSP_66_LE_ELF.out: Load failed.
 
请问是不是我的CMD文件中DDR3的定义有问题?还是GEL文件有问题?网上也有人说是C6678无法load外部扩展的DDR3等等。。。
  • 使用MCSDK中提供的GEL文件,加载GEL后,可以将程序load到外部DDR3。

    你使用FFT点数为4K,8K和16K时,load到DDR3中有问题吗?

  • 求解load 在CMD文件中定义数据段时的具体含义

    现在4K,8K,6K,64k时,都可以load到DDR3中,但是存在以下问题:在定义DDR3段时,用不用load语句,指令运行周期数差别比较大,请大神分析原因。

    以64k的复数浮点FFT为例,

    定义DDR3段的时候采用.DDR3:load>>DDR3 采用load指令时指令周期数CYCLES:3096024

    定义DDR3段的时候采用.DDR3:>>DDR3没有采用load指令时指令周期数CYCLES:54106352

    相差数十倍,求原因。

    测试结果如下:
     数据存放在DDR3中 定义DDR3段的时候采用.DDR3:load>>DDR3 采用load指令        

     FFT点数                         运行时间                运行指令周期数数  

    N = 8   radix = 2  TIME: 0.215000 us  CYCLES:215

     N = 16   radix = 4  TIME: 0.243000 us  CYCLES:243  

    N = 32   radix = 2  TIME: 0.401000 us  CYCLES:401  

    N = 64   radix = 4  TIME: 0.617000 us  CYCLES:617

     N = 128  radix = 2  TIME: 1.207000 us  CYCLES:1207

     N = 256  radix = 4  TIME: 2.168000 us  CYCLES:2168  

    N = 512  radix = 2  TIME: 4.793000 us  CYCLES:4793

     N = 1024  radix = 4  TIME: 9.256000 us  CYCLES:9256  

    N = 2048  radix = 2  TIME: 21.034000 us  CYCLES:21034

    N = 4096  radix = 4  TIME: 51.208000 us  CYCLES:51208  

    N = 8192  radix = 2  TIME: 266.581000 us  CYCLES:266581  

    N = 16384  radix = 4  TIME: 539.959000 us  CYCLES:539959  

    N = 32768  radix = 2  TIME: 1512.223000 us  CYCLES:1512223  

    N = 65536  radix = 4  TIME: 3096.024000 us  CYCLES:3096024

     数据存放在DDR3中 定义DDR3段的时候采用.DDR3:>>DDR3没有采用load指令        

    FFT点数                         运行时间                运行指令周期数数  

    N = 8   radix = 2  TIME: 1.603000 us  CYCLES:1603  

    N = 16   radix = 4  TIME: 3.136000 us  CYCLES:3136  

    N = 32   radix = 2  TIME: 9.645000 us  CYCLES:9645  

    N = 64   radix = 4  TIME: 19.355000 us  CYCLES:19355  

    N = 128  radix = 2  TIME: 52.260000 us  CYCLES:52260  

    N = 256  radix = 4  TIME: 104.660000 us  CYCLES:104660  

    N = 512  radix = 2  TIME: 260.284000 us  CYCLES:260284  

    N = 1024  radix = 4  TIME: 480.613000 us  CYCLES:480613  

    N = 2048  radix = 2  TIME: 1040.438000 us  CYCLES:1040438  

    N = 4096  radix = 4  TIME: 2064.545000 us  CYCLES:2064545  

    N = 8192  radix = 2  TIME: 4781.424000 us  CYCLES:4781424  

    N = 16384  radix = 4  TIME: 10776.016000 us  CYCLES:10776016  

    N = 32768  radix = 2  TIME: 25084.586000 us  CYCLES:25084586  

    N = 65536  radix = 4  TIME: 54106.352000 us  CYCLES:54106352

  • 你好,cmd中的load是一个关键字,并不是指令。此关键字可以省略。

    具体能把你的CMD文件贴上来看看有什么不一样吗?

  • 两种情况的cmd文件仅仅在定义段.DDR3时加与,不加load

    定义段.DDR3时,加load的CMD文件

    -heap  0x8000 -stack 0xC000

    MEMORY {   

      L2SRAM (RWX) : org = 0x800000, len = 0x100000    

     MSMCSRAM (RWX) : org = 0xc000000, len = 0x200000    

    DDR3(RWX)    :  org = 0x80000000,len = 0x10000000

     }

    SECTIONS {   

      .kernel: {      

      *.obj (.text:optimized) { SIZE(_kernel_size) }    

    }

      .text: load >> L2SRAM    

     .text:touch: load >> L2SRAM        

     GROUP (NEAR_DP)   

      {    

     .neardata     .rodata     .bss    

     } load > L2SRAM

        .far: load >> L2SRAM    

     .fardata: load >> L2SRAM    

    .data: load >> L2SRAM    

    .switch: load >> L2SRAM    

     .stack: load > L2SRAM    

    .args: load > L2SRAM align = 0x4, fill = 0 {_argsize = 0x200; }    

    .sysmem: load > L2SRAM    

     .cinit: load > L2SRAM    

    .const: load > L2SRAM START(const_start) SIZE(const_size)    

    .pinit: load > L2SRAM     .

    cio: load >> L2SRAM    

    xdc.meta: load >> L2SRAM, type = COPY    

     //.MSMCSRAM: >> MSMCSRAM    

    .DDR3:load>> DDR3

    }

    定义段.DDR3时,不加load的CMD文件

    -heap  0x8000 -stack 0xC000

    MEMORY {  

      L2SRAM (RWX) : org = 0x800000, len = 0x100000   

    MSMCSRAM (RWX) : org = 0xc000000, len = 0x200000    

    DDR3(RWX)    :  org = 0x80000000,len = 0x10000000

    }

    SECTIONS {  

      .kernel: {     

      *.obj (.text:optimized) { SIZE(_kernel_size) }    

    }

      .text: load >> L2SRAM   

    .text:touch: load >> L2SRAM        

    GROUP (NEAR_DP)  

      {   

    .neardata     .rodata     .bss   

    } load > L2SRAM

        .far: load >> L2SRAM   

    .fardata: load >> L2SRAM    

    .data: load >> L2SRAM    

    .switch: load >> L2SRAM   

    .stack: load > L2SRAM    

    .args: load > L2SRAM align = 0x4, fill = 0 {_argsize = 0x200; }    

    .sysmem: load > L2SRAM   

    .cinit: load > L2SRAM    

    .const: load > L2SRAM START(const_start) SIZE(const_size)    

    .pinit: load > L2SRAM     .

    cio: load >> L2SRAM    

    xdc.meta: load >> L2SRAM, type = COPY   

    //.MSMCSRAM: >> MSMCSRAM    

    .DDR3:>> DDR3

    }

  • 我有一个相似的问题需要解决:

    TMS320C671X: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x1e40: This operation is not supported by this driver
    TMS320C671X: GEL: File: C:\Users\WangXi\workspace_v6_0\Sinebuf\Release\Sinebuf.out: Load failed.

    你们有什么好的解决方法吗