This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467内核启动Sending DHCP and RARP requests ....time out!

 

升级DVSDK 2.0过程中启动新内核报错,详见下方启动信息

U-Boot 1.2.0 (May 20 2009 - 01:04:07)

 

I2C:   ready

DRAM:  256 MB

unknown vendor=0 Flash:  0 kB

NAND:  NAND device: Manufacturer ID: 0x20, Chip ID: 0x76 (ST Micro NAND 64MiB 3,

3V 8-bit)

64 MiB

*** Warning - bad CRC or NAND, using default environment

 

In:    serial

Out:   serial

Err:   serial

ARM Clock :- 297MHz

DDR Clock :- 297MHz

Hit any key to stop autoboot:  0

DM6467 HD EVM # setenv serverip 10.78.86.60

DM6467 HD EVM # setenv ipaddr 10.78.86.69

DM6467 HD EVM # tftp 80700000 uImage

TFTP from server 10.78.86.60; our IP address is 10.78.86.69

Filename 'uImage'.

Load address: 0x80700000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ################################################################

done

Bytes transferred = 1988232 (1e5688 hex)

DM6467 HD EVM # bootm

## Booting image at 80700000 ...

   Image Name:   Linux-2.6.18_pro500-davinci_evm-

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    1988168 Bytes =  1.9 MB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

OK

 

Starting kernel ...

 

Uncompressing Linux.............................................................

...................................................................... done, boo

ting the kernel.

Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (davinci@davinci-desktop) (gc

c 版本 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Fri May

 17 17:39:08 CST 2013

CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177

Machine: DaVinci DM6467 EVM

Memory policy: ECC disabled, Data cache writeback

DaVinci DM6467 variant 0x0

CPU0: D VIVT write-back cache

CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets

CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets

Built 1 zonelists.  Total pages: 30720

Kernel command line: console=ttyS0,115200n8 noinitrd rw root=/dev/nfs nfsroot=19

2.168.1.101:/opt/montavista/pro/devkit/arm/v5t_le/target,nolock mem=120M

PID hash table entries: 512 (order: 9, 2048 bytes)

Clock event device timer0_0 configured with caps set: 03

Console: colour dummy device 80x30

Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)

Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)

Memory: 120MB = 120MB total

Memory: 117504KB available (3401K code, 684K data, 172K init)

Security Framework v1.0.0 initialized

Capability LSM initialized

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

NET: Registered protocol family 16

DaVinci: 48 gpio irqs

ch0 default output "COMPOSITE", mode "NTSC"

ch1 default output "", mode ""

SCSI subsystem initialized

usbcore: registered new driver usbfs

usbcore: registered new driver hub

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 4096 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 4096 bind 2048)

TCP reno registered

VFS: Disk quotas dquot_6.5.1

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

squashfs: version 3.1 (2006/08/19) Phillip Lougher

JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.

yaffs May 17 2013 17:36:24 Installing.

SGI XFS with no debug enabled

Initializing Cryptographic API

io scheduler noop registered

io scheduler anticipatory registered (default)

LTT : ltt-facilities init

LTT : ltt-facility-core init in kernel

DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec

CIR device registered successfully (Major = 252, Minor = 0)

Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled

serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a ST16654

 

serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfec20400 (irq = 41) is a ST16650

V2

serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ4

2): -28

RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize

netconsole: not configured, aborting

TI DaVinci EMAC: MAC address is 00:0e:99:50:44:02

TI DaVinci EMAC Linux version updated 4.0

TI DaVinci EMAC: Installed 1 instances.

Linux video capture interface: v2.00

i2c /dev entries driver

Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2

ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx

MUX: initialized ATAEN

    ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio

hda: HP J7948G, ATA DISK drive

ide0 at 0xfec661f0-0xfec661f7,0xfec663f6 on irq 22

hda: max request size: 512KiB

hda: 156301488 sectors (80026 MB) w/8192KiB Cache, CHS=16383/255/63, UDMA(66)

hda: cache flushes supported

 hda: hda1 hda2

Initializing USB Mass Storage driver...

usbcore: registered new driver usb-storage

USB Mass Storage support registered.

usbcore: registered new driver usbhid

drivers/usb/input/hid-core.c: v2.6:USB HID core driver

musb_hdrc: version 6.0, cppi-dma, host, debug=0

musb_hdrc: USB Host mode controller at c805c000 using DMA, IRQ 13

musb_hdrc musb_hdrc: MUSB HDRC host driver

musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mice: PS/2 mouse device common for all mice

Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50

2006 UTC).

ASoC version 0.13.1

AIC3X Audio Codec 0.1

asoc: aic3x <-> davinci-i2s mapping ok

asoc: DIT <-> davinci-dit mapping ok

ALSA device list:

  #0: DaVinci DM6467 EVM (aic3x)

IPv4 over IPv4 tunneling driver

TCP bic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

Time: timer0_1 clocksource has been installed.

Clock event device timer0_0 configured with caps set: 08

Switched to high resolution mode on CPU 0

Sending DHCP and RARP requests ....