This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求解NDK中例程hello world运行以太网测试程序问题?



 

1.测试平台C6678LE EVM开发板   ,测试例程为:MCSDK 目录下NDK中的hello world工程

2.测试目标:C6678LE EVM开发板与PC机进行以太网通信

存在以下4个问题请大家帮忙解答,具体问题在请看帖内,谢谢!

开发板的IP信息配置为:

hello world 源文件中的IP信息如下

char *HostName    = "tidsp";

char *LocalIPAddr = "192.168.2.100";

char *LocalIPMask = "255.255.255.0";    // Not used when using DHCP

char *GatewayIP   =  "192.168.2.101";    // Not used when using DHCP

char *DomainName  = "demo.net";         // Not used when using DHCP

char *DNSServer   = "0.0.0.0";          // Used when set to anything but zero、

PC机的IP地址为:192.168.2.50

问题一:我配置的开发板与PC机IP信息对吗?

在PC机上ping开发板的IP地址结果如下图所示:

 

问题二:如上图所示,出现“无法访问目标主机”,但是ping结果4个数据包全部接收,不存在丢包现象,请问这种情况下是不是PC机与开发板的是以太网已经连接?出新这种情况的原因是什么?

debug运行会在控制台上打印以下信息,出现两种情况:

第一种情况:

[C66xx_0] QMSS successfully initialized

[C66xx_0] CPPI successfully initialized

[C66xx_0] PA successfully initialized

[C66xx_0] [C66xx_0] TCP/IP Stack 'Hello World!' Application

[C66xx_0]

[C66xx_0]

[C66xx_0] TCP/IP Stack 'Hello World!' Application

[C66xx_0]

[C66xx_0] PASS successfully initialized

[C66xx_0] Ethernet subsystem successfully initialized

[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7

[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 911, found 1 entries

[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 913, found 1 entries

[C66xx_0] Registration of the EMAC Successful, waiting for link up ..

[C66xx_0] Service Status: DHCPC    : Enabled  :          : 000

[C66xx_0] Service Status: DHCPC    : Enabled  : Running  : 000

问题三:上面的控制台打印信息是不是说明以太网已经可以与PC机通信了?

第二种情况:

[C66xx_0] QMSS successfully initialized

[C66xx_0] CPPI successfully initialized

[C66xx_0] PA successfully initialized

[C66xx_0]

[C66xx_0] TCP/IP Stack 'Hello World!' Application

[C66xx_0]

[C66xx_0]

[C66xx_0] TCP/IP Stack 'Hello World!' Application

[C66xx_0] [C66xx_0] PASS successfully initialized

[C66xx_0] Ethernet subsystem successfully initialized

[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7

[C66xx_0] Timeout waiting for reply from PA to Pa_addMac command

[C66xx_0] Add_MACAddress failed [C66xx_0] Error: Unable to register the EMAC

[C66xx_0] NIMUIOCTL Failed with error code: -22

[C66xx_0] Service Status: DHCPC    : Failed   :          : 000

问题四:上面的控制台打印信息是不是说明以太网已经无法与PC机通信了?如何进行修改?