1.测试平台C6678LE EVM开发板 ,测试例程为:MCSDK 目录下NDK中的hello world工程
2.测试目标:C6678LE EVM开发板与PC机进行以太网通信
存在以下4个问题请大家帮忙解答,具体问题在请看帖内,谢谢!
开发板的IP信息配置为:
hello world 源文件中的IP信息如下
char *HostName = "tidsp";
char *LocalIPAddr = "192.168.2.100";
char *LocalIPMask = "255.255.255.0"; // Not used when using DHCP
char *GatewayIP = "192.168.2.101"; // Not used when using DHCP
char *DomainName = "demo.net"; // Not used when using DHCP
char *DNSServer = "0.0.0.0"; // Used when set to anything but zero、
PC机的IP地址为:192.168.2.50
问题一:我配置的开发板与PC机IP信息对吗?
在PC机上ping开发板的IP地址结果如下图所示:
问题二:如上图所示,出现“无法访问目标主机”,但是ping结果4个数据包全部接收,不存在丢包现象,请问这种情况下是不是PC机与开发板的是以太网已经连接?出新这种情况的原因是什么?
第一种情况:
[C66xx_0] QMSS successfully initialized
[C66xx_0] CPPI successfully initialized
[C66xx_0] PA successfully initialized
[C66xx_0] [C66xx_0] TCP/IP Stack 'Hello World!' Application
[C66xx_0]
[C66xx_0]
[C66xx_0] TCP/IP Stack 'Hello World!' Application
[C66xx_0]
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7
[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 911, found 1 entries
[C66xx_0] Verify_Init: Expected 0 entry count for Queue number = 913, found 1 entries
[C66xx_0] Registration of the EMAC Successful, waiting for link up ..
[C66xx_0] Service Status: DHCPC : Enabled : : 000
[C66xx_0] Service Status: DHCPC : Enabled : Running : 000
问题三:上面的控制台打印信息是不是说明以太网已经可以与PC机通信了?
第二种情况:
[C66xx_0] QMSS successfully initialized
[C66xx_0] CPPI successfully initialized
[C66xx_0] PA successfully initialized
[C66xx_0]
[C66xx_0] TCP/IP Stack 'Hello World!' Application
[C66xx_0]
[C66xx_0]
[C66xx_0] TCP/IP Stack 'Hello World!' Application
[C66xx_0] [C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7
[C66xx_0] Timeout waiting for reply from PA to Pa_addMac command
[C66xx_0] Add_MACAddress failed [C66xx_0] Error: Unable to register the EMAC
[C66xx_0] NIMUIOCTL Failed with error code: -22
[C66xx_0] Service Status: DHCPC : Failed : : 000
问题四:上面的控制台打印信息是不是说明以太网已经无法与PC机通信了?如何进行修改?