This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error:failed to create capture device

您好,我按照software guide运行demo时,使用命令./encodedecode -b 2000000 -v h264 -k -I 4

得到下面的错误:

Encodedecode demo started.

davinci_resizer davinci_resizer.2:RSZ_G_CONFIG:0:0:124

davinci_previewer davinci_previewer.2:ipipe_set_preview_config

davinci_previewer davinci_previewer.2:ipipe_set_preview_config

vpfe-capture vpfe-capture:IPIPE Chained

vpfe-capture vpfe-capture:Resizer present

Error:Failed to create capture device

我的 bootargs :

setenv bootargs 'console=ttyS0,115200n8 noinitrd rw ip=192.168.1.166 root=/dev/nfs nfsroot=192.168.1.111:/root/targetfs,nolock mem=60M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4'

请问问题出在哪里?

谢谢

  • 你好,

    请问你使用的芯片具体是哪颗?是DM36x么?

    请问你使用的硬件是芯片官方的评估板么?

    在代码里面加点打印在定位一下。

  • 我使用的是DM368,使用的硬件是EVM DM368,运行的是SDK中的demo encodedecode,没有修改,刚开始研究,请问应该在哪部分代码中加打印?