This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error:failed to create capture device



您好,我按照software guide运行demo时,使用命令./encodedecode -b 2000000 -v h264 -k -I 4

得到下面的错误:

Encodedecode demo started.

davinci_resizer davinci_resizer.2:RSZ_G_CONFIG:0:0:124

davinci_previewer davinci_previewer.2:ipipe_set_preview_config

davinci_previewer davinci_previewer.2:ipipe_set_preview_config

vpfe-capture vpfe-capture:IPIPE Chained

vpfe-capture vpfe-capture:Resizer present

Error:Failed to create capture device

我的 bootargs :

setenv bootargs 'console=ttyS0,115200n8 noinitrd rw ip=192.168.1.166 root=/dev/nfs nfsroot=192.168.1.111:/root/targetfs,nolock mem=60M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4'

请问问题出在哪里?

谢谢