This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320VC5509A: 采用McBSP的时间停止模式,将dsp配置位SPI从设备,用DMA传递数据,出现一次接收(或发送)无法得到全部数据的情况

Part Number: TMS320VC5509A

系统:

stm32为ti模式的spi主机,dsp为spi从机,两者都使用dma,

具体问题:

1.主机发送从机接收:上电后,主机第一次发送1024个16位的数据,从机(dsp)接收到1023个数据(这些数据没有问题),在下一次传输开始后,接收到最后一个数据,并产生中断,并在处理完中断事件后,进行下一次的接收,即再次接收1023点,后等待下一次数据传输;经过验证,最后一位数据确实为上一次发送的最后一位数据。

2.从机发送主机接收:上电后,在主机开启第一次发送后,从机开启发送,从主机的接收数据中可以看出,其与发送结果一致;当开始下一次传输时,主机先会接收到上一次传输的两个尾部数据,并且其中的第二个数据为0x0000,其余数据值正常,出现位置依次错位;在进行第三次传输时,主机先会接收到上一次传输的三个尾部数据,其余数据值正常,出现位置依次错位;应该也与‘1’中的原因类似,相当于两次发送产生一次接收,只是错位数据量不同。

3.个人感觉应该是dma配置的问题,希望各位大佬能帮帮忙。

dsp端的代码:

/*
 * main.c
 */

#include <stdio.h>
//#define  CHIP_5509A

#include <csl.h>
#include <csl_pll.h>
#include <csl_chip.h>
#include <csl_gpio.h>
#include <csl_mcbsp.h>
#include <math.h>
#include <tms320.h>
#include <stdio.h>
#include <csl_dma.h>
#include <csl_irq.h>
#include <dsplib.h>


#define N       1024
#define N2      1024


//---------Global data definition---------

/* Define transmit and receive buffers */
#pragma DATA_SECTION(xmt,".dmaMem")
DATA xmt[N2];
#pragma DATA_SECTION(xmtB,".dmaMem")
DATA xmtB[N2];
#pragma DATA_SECTION(rcv,".dmaMem")
DATA rcv[N];
#pragma DATA_SECTION(rcvB,".dmaMem2")
DATA rcvB[N];

// PLL 初始化结构体
PLL_Config  myConfig      = {
  0,    //IAI: the PLL locks using the same process that was underway
                //before the idle mode was entered
  1,    //IOB: If the PLL indicates a break in the phase lock,
                //it switches to its bypass mode and restarts the PLL phase-locking
                //sequence
  24,    //PLL multiply value; multiply 24 times
  1             //Divide by 2 PLL divide value; it can be either PLL divide value
                //(when PLL is enabled), or Bypass-mode divide value
                //(PLL in bypass mode, if PLL multiply value is set to 1)
};


//McBSP 对应结构体以及初始化
MCBSP_Config ConfigLoopBack16= {
MCBSP_SPCR1_RMK(
  MCBSP_SPCR1_DLB_OFF,                    /* DLB    = 0 */
  MCBSP_SPCR1_RJUST_RZF,                 /* RJUST  = 0 */
  MCBSP_SPCR1_CLKSTP_NODELAY,            /* CLKSTP = 0 */ //MCBSP_SPCR1_CLKSTP_NODELAY
  MCBSP_SPCR1_DXENA_NA,                  /* DXENA  = 0 */
  MCBSP_SPCR1_ABIS_DISABLE,              /* ABIS   = 0 */
  MCBSP_SPCR1_RINTM_RRDY,                /* RINTM  = 0 */
  0,                                     /* RSYNCER = 0 */
  MCBSP_SPCR1_RRST_DISABLE               /* RRST   = 0 */
 ),
  MCBSP_SPCR2_RMK(
  MCBSP_SPCR2_FREE_NO,                   /* FREE   = 0 */
  MCBSP_SPCR2_SOFT_NO,                   /* SOFT   = 0 */
  MCBSP_SPCR2_FRST_FSG,                  /* FRST   = 0 */
  MCBSP_SPCR2_GRST_CLKG,                 /* GRST   = 0 */
  MCBSP_SPCR2_XINTM_XRDY,                /* XINTM  = 0 */
  0,                                     /* XSYNCER = N/A */
  MCBSP_SPCR2_XRST_DISABLE               /* XRST   = 0 */
 ),
MCBSP_RCR1_RMK(
MCBSP_RCR1_RFRLEN1_OF(0),                /* RFRLEN1 = 0 */
MCBSP_RCR1_RWDLEN1_16BIT                 /* RWDLEN1 = 5 */
),
MCBSP_RCR2_RMK(
  MCBSP_RCR2_RPHASE_SINGLE,              /* RPHASE  = 0 */
  MCBSP_RCR2_RFRLEN2_OF(0),              /* RFRLEN2 = 0 */
  MCBSP_RCR2_RWDLEN2_16BIT,               /* RWDLEN2 = 0 */
  MCBSP_RCR2_RCOMPAND_MSB,               /* RCOMPAND = 0 */
  MCBSP_RCR2_RFIG_YES,                   /* RFIG    = 0 */
  MCBSP_RCR2_RDATDLY_0BIT                /* RDATDLY = 0 */
  ),
 MCBSP_XCR1_RMK(
  MCBSP_XCR1_XFRLEN1_OF(0),              /* XFRLEN1 = 0 */
  MCBSP_XCR1_XWDLEN1_16BIT               /* XWDLEN1 = 5 */

),
MCBSP_XCR2_RMK(
  MCBSP_XCR2_XPHASE_SINGLE,              /* XPHASE  = 0 */
  MCBSP_XCR2_XFRLEN2_OF(0),              /* XFRLEN2 = 0 */
  MCBSP_XCR2_XWDLEN2_16BIT,               /* XWDLEN2 = 0 */
  MCBSP_XCR2_XCOMPAND_MSB,               /* XCOMPAND = 0 */
  MCBSP_XCR2_XFIG_YES,                   /* XFIG    = 0 */
  MCBSP_XCR2_XDATDLY_0BIT                /* XDATDLY = 0 */
),
MCBSP_SRGR1_RMK(
 MCBSP_SRGR1_FWID_OF(1),                /* FWID    = 1 */
 MCBSP_SRGR1_CLKGDV_OF(1)               /* CLKGDV  = 1 */
),
MCBSP_SRGR2_RMK(
  MCBSP_SRGR2_GSYNC_FREE,                /* FREE    = 0 */
  MCBSP_SRGR2_CLKSP_RISING,              /* CLKSP   = 0 */
  MCBSP_SRGR2_CLKSM_INTERNAL,            /* CLKSM   = 1 */
  MCBSP_SRGR2_FSGM_DXR2XSR,              /* FSGM    = 0 */
  MCBSP_SRGR2_FPER_OF(15)                /* FPER    = 0 */
),
MCBSP_MCR1_DEFAULT,
MCBSP_MCR2_DEFAULT,
MCBSP_PCR_RMK(
 MCBSP_PCR_IDLEEN_RESET,                 /* IDLEEN   = 0   */
 MCBSP_PCR_XIOEN_SP,                     /* XIOEN    = 0   */
 MCBSP_PCR_RIOEN_SP,                     /* RIOEN    = 0   */
 MCBSP_PCR_FSXM_EXTERNAL,                /* FSXM     = 0   */
 MCBSP_PCR_FSRM_EXTERNAL,                /* FSRM     = 0   */
 MCBSP_PCR_CLKXM_INPUT,                 /* CLKXM    = 0   */
 MCBSP_PCR_CLKRM_OUTPUT,                  /* CLKRM    = 1   */
 MCBSP_PCR_SCLKME_NO,                    /* SCLKME   = 0   */
 0,                                      /* DXSTAT = N/A   */
 MCBSP_PCR_FSXP_ACTIVELOW,   //LOW =1       /* FSXP     = 0   */
 MCBSP_PCR_FSRP_ACTIVELOW,              /* FSRP     = 0   */
 MCBSP_PCR_CLKXP_RISING,  // RISING     /* CLKXP    = 0   */ //1;MCBSP_PCR_CLKXP_RISING
 MCBSP_PCR_CLKRP_RISING//FALLING         /* CLKRP    = 0   */ //1
),
MCBSP_RCERA_DEFAULT,
MCBSP_RCERB_DEFAULT,
MCBSP_RCERC_DEFAULT,
MCBSP_RCERD_DEFAULT,
MCBSP_RCERE_DEFAULT,
MCBSP_RCERF_DEFAULT,
MCBSP_RCERG_DEFAULT,
MCBSP_RCERH_DEFAULT,
MCBSP_XCERA_DEFAULT,
MCBSP_XCERB_DEFAULT,
MCBSP_XCERC_DEFAULT,
MCBSP_XCERD_DEFAULT,
MCBSP_XCERE_DEFAULT,
MCBSP_XCERF_DEFAULT,
MCBSP_XCERG_DEFAULT,
MCBSP_XCERH_DEFAULT
};


//DMA
/* Create DMA Receive Side Configuration */
DMA_Config  dmaRcvConfig = {
  DMA_DMACSDP_RMK(
    DMA_DMACSDP_DSTBEN_NOBURST,
    DMA_DMACSDP_DSTPACK_OFF,
    DMA_DMACSDP_DST_DARAM,
    DMA_DMACSDP_SRCBEN_NOBURST,
    DMA_DMACSDP_SRCPACK_OFF,
    DMA_DMACSDP_SRC_PERIPH,
    DMA_DMACSDP_DATATYPE_16BIT
  ),                                       /* DMACSDP  */
  DMA_DMACCR_RMK(
    DMA_DMACCR_DSTAMODE_POSTINC,
    DMA_DMACCR_SRCAMODE_CONST,
    DMA_DMACCR_ENDPROG_ON,
    DMA_DMACCR_REPEAT_OFF,/****20220401****/
    DMA_DMACCR_AUTOINIT_ON,/****20220401****/
    DMA_DMACCR_EN_STOP,
    DMA_DMACCR_PRIO_LOW,
    DMA_DMACCR_FS_DISABLE,
    DMA_DMACCR_SYNC_REVT1
  ),                                       /* DMACCR   */
  DMA_DMACICR_RMK(
    DMA_DMACICR_BLOCKIE_OFF,
    DMA_DMACICR_LASTIE_OFF,
    DMA_DMACICR_FRAMEIE_ON,
    DMA_DMACICR_FIRSTHALFIE_OFF,
    DMA_DMACICR_DROPIE_OFF,
    DMA_DMACICR_TIMEOUTIE_OFF
  ),                                       /* DMACICR  */
    (DMA_AdrPtr)(MCBSP_ADDR(DRR11)),        /* DMACSSAL */
    0,                                     /* DMACSSAU */
    0,                     				   /* DMACDSAL */ //在后面进行了赋值
    0,                                     /* DMACDSAU */
    N,                                     /* DMACEN   */
    1,                                     /* DMACFN   */
    0,                                     /* DMACFI  */
    0                                      /* DMACEI  */
  };

/* Create DMA Transmit Side Configuration */
DMA_Config  dmaXmtConfig = {
  DMA_DMACSDP_RMK(
    DMA_DMACSDP_DSTBEN_NOBURST,
    DMA_DMACSDP_DSTPACK_OFF,
    DMA_DMACSDP_DST_PERIPH,
    DMA_DMACSDP_SRCBEN_NOBURST,
    DMA_DMACSDP_SRCPACK_OFF,
    DMA_DMACSDP_SRC_DARAM,
    DMA_DMACSDP_DATATYPE_16BIT
  ),                                       /* DMACSDP  */
  DMA_DMACCR_RMK(
    DMA_DMACCR_DSTAMODE_CONST,
    DMA_DMACCR_SRCAMODE_POSTINC,
    DMA_DMACCR_ENDPROG_ON,
    DMA_DMACCR_REPEAT_OFF,/****20220401****/
    DMA_DMACCR_AUTOINIT_ON,/****20220401****/
    DMA_DMACCR_EN_STOP,
    DMA_DMACCR_PRIO_LOW,
    DMA_DMACCR_FS_DISABLE,
    DMA_DMACCR_SYNC_XEVT1
  ),                                       /* DMACCR   */
  DMA_DMACICR_RMK(
    DMA_DMACICR_BLOCKIE_OFF,
    DMA_DMACICR_LASTIE_OFF,
    DMA_DMACICR_FRAMEIE_ON,
    DMA_DMACICR_FIRSTHALFIE_OFF,
    DMA_DMACICR_DROPIE_OFF,
    DMA_DMACICR_TIMEOUTIE_OFF
  ),                                       /* DMACICR  */
    0,                  				   /* DMACSSAL */ //在后面进行了赋值
    0,                                     /* DMACSSAU */
    (DMA_AdrPtr)(MCBSP_ADDR(DXR11)),       /* DMACDSAL */
    0,                                     /* DMACDSAU */
    N2,                                     /* DMACEN   */
    1,                                     /* DMACFN   */
    0,                                     /* DMACFI   */
    0                                      /* DMACEI   */
};


/* Define a DMA_Handle object to be used with DMA_open function */
DMA_Handle hDmaRcv, hDmaXmt;

/* Define a MCBSP_Handle object to be used with MCBSP_open function */
MCBSP_Handle hMcbsp;

volatile Uint16 receiveComplete = FALSE;
volatile Uint16 transmitComplete = FALSE;

volatile Uint16 rbflg = 0;
Uint16 err = 0;
Uint16 old_intm;
Uint16 xmtEventId, rcvEventId;

Uint16 runtimeX=0,runtimeR=0;
//---------Function prototypes---------
/* Reference start of interrupt vector table   */
/* This symbol is defined in file, vectors.s55 */
extern void VECSTART(void);

/* Protoype for interrupt functions */
interrupt void dmaXmtIsr(void);
interrupt void dmaRcvIsr(void);
void taskFxn(void);

void main(void)
{
    Uint16 i;

    /* Initialize CSL library - This is REQUIRED !!! */
    CSL_init();

    /* Set IVPD/IVPH to start of interrupt vector table */
    IRQ_setVecs((Uint32)(&VECSTART));
    PLL_config(&myConfig);

    for (i = 0; i <= N - 1; i++) {
        rcv[i] = 0;
        rcvB[i] = 0;
    }
    for (i = 0; i <= N; i++) {
        xmt[i] = N-i;
        xmtB[i] = N-i;
    }

    /* Call function to effect transfer */

        taskFxn();
}


void taskFxn(void)
{
    Uint16 srcAddrHi, srcAddrLo;
    Uint16 dstAddrHi, dstAddrLo;
    Uint16 i;

    /* By default, the TMS320C55xx compiler assigns all data symbols word */
    /* addresses. The DMA however, expects all addresses to be byte       */
    /* addresses. Therefore, we must shift the address by 2 in order to   */
    /* change the word address to a byte address for the DMA transfer.    */
    srcAddrHi = (Uint16)(((Uint32)(MCBSP_ADDR(DRR11))) >> 15) & 0xFFFFu;
    srcAddrLo = (Uint16)(((Uint32)(MCBSP_ADDR(DRR11))) << 1) & 0xFFFFu;
    dstAddrHi = (Uint16)(((Uint32)(rcv)) >> 15) & 0xFFFFu;
    dstAddrLo = (Uint16)(((Uint32)(rcv)) << 1) & 0xFFFFu;

    dmaRcvConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
    dmaRcvConfig.dmacssau = srcAddrHi;
    dmaRcvConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
    dmaRcvConfig.dmacdsau = dstAddrHi;

    srcAddrHi = (Uint16)(((Uint32)(xmt)) >> 15) & 0xFFFFu;
    srcAddrLo = (Uint16)(((Uint32)(xmt)) << 1) & 0xFFFFu;
    dstAddrHi = (Uint16)(((Uint32)(MCBSP_ADDR(DXR11))) >> 15) & 0xFFFFu;
    dstAddrLo = (Uint16)(((Uint32)(MCBSP_ADDR(DXR11))) << 1) & 0xFFFFu;

    dmaXmtConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
    dmaXmtConfig.dmacssau = srcAddrHi;
    dmaXmtConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
    dmaXmtConfig.dmacdsau = dstAddrHi;



    /* Open DMA channels 4 & 5 and set regs to power on defaults */
    hDmaRcv = DMA_open(DMA_CHA4,DMA_OPEN_RESET);
    hDmaXmt = DMA_open(DMA_CHA5,DMA_OPEN_RESET);

    /* Open MCBSP Port 1 and set registers to their power on defaults */
    hMcbsp = MCBSP_open(MCBSP_PORT1, MCBSP_OPEN_RESET);


    /* Get interrupt event associated with DMA receive and transmit */
    xmtEventId = DMA_getEventId(hDmaXmt);
    rcvEventId = DMA_getEventId(hDmaRcv);

    /* Temporarily disable interrupts and clear any pending */
    /* interrupts for MCBSP transmit */
    old_intm = IRQ_globalDisable();

    /* Clear any pending interrupts for DMA channels */
    IRQ_clear(xmtEventId);
    IRQ_clear(rcvEventId);

    /* Enable DMA interrupt in IER register */
    IRQ_enable(xmtEventId);
    IRQ_enable(rcvEventId);

    /* Set Start Of Interrupt Vector Table */
    IRQ_setVecs(0x10000);

    /* Place DMA interrupt service addresses at associate vector */
    IRQ_plug(xmtEventId,&dmaXmtIsr);
    IRQ_plug(rcvEventId,&dmaRcvIsr);



    /* Write values from configuration structure to DMA control regs */
    DMA_config(hDmaRcv,&dmaRcvConfig);
    DMA_config(hDmaXmt,&dmaXmtConfig);

    /* Write values from configuration structure to MCBSP control regs */
    MCBSP_config(hMcbsp, &ConfigLoopBack16);


    /* Enable all maskable interrupts */
    IRQ_globalEnable();

    /* Enable DMA */
    DMA_start(hDmaRcv);
    DMA_start(hDmaXmt);

    /* Start Sample Rate Generator and Enable Frame Sync */
    MCBSP_start(hMcbsp,
            MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC,
            0x30u);

    /* Take MCBSP transmit and receive out of reset */
    MCBSP_start(hMcbsp,
            MCBSP_XMIT_START | MCBSP_RCV_START,
            0u);

    while(1)
    {
        /* Wait for DMA transfer to be complete */
        while (!receiveComplete){}//等待接收完成
        while (!transmitComplete){}//

        while(DMA_FGETH(hDmaRcv, DMACCR, ENDPROG));

            dstAddrHi = (Uint16)(((Uint32)(rcv)) >> 15) & 0xFFFFu;
            dstAddrLo = (Uint16)(((Uint32)(rcv)) << 1) & 0xFFFFu;
            DMA_RSETH(hDmaRcv, DMACDSAU, dstAddrHi);
            DMA_RSETH(hDmaRcv, DMACDSAL, dstAddrLo);

        DMA_RSETH(hDmaRcv, DMACEN,N);
        DMA_RSETH(hDmaRcv, DMACFN,1);

        DMA_FSETH(hDmaRcv, DMACCR, ENDPROG,1);


        while(DMA_FGETH(hDmaXmt, DMACCR, ENDPROG));

        for(i=0;i<N2;i++) xmt[i]=xmt[i]+8;

            srcAddrHi = (Uint16)(((Uint32)(xmt)) >> 15) & 0xFFFFu;
            srcAddrLo = (Uint16)(((Uint32)(xmt)) << 1) & 0xFFFFu;
            DMA_RSETH(hDmaXmt, DMACSSAU, srcAddrHi);
            DMA_RSETH(hDmaXmt, DMACSSAL, srcAddrLo);


        DMA_RSETH(hDmaXmt, DMACEN,N2);
        DMA_RSETH(hDmaXmt, DMACFN,1);

        DMA_FSETH(hDmaXmt, DMACCR, ENDPROG,1);


        receiveComplete = FALSE;
        transmitComplete = FALSE;


    }
    /* Restore status of global interrupt enable flag */
    IRQ_globalRestore(old_intm);

    /* We're done with MCBSP and DMA , so close them */
    MCBSP_close(hMcbsp);
    DMA_close(hDmaRcv);
    DMA_close(hDmaXmt);
}



interrupt void dmaXmtIsr(void) {
	runtimeX++;//记录中断触发次数

    transmitComplete = TRUE;
    DMA_FSETH(hDmaXmt, DMACSR, FRAME,0);
}

interrupt void dmaRcvIsr(void) {
	runtimeR++;

    receiveComplete = TRUE;
    DMA_FSETH(hDmaRcv, DMACSR, FRAME,0);
}