This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713B: MCBSP配置成SPI主模式和2个SPI从设备通信,这2个设备的CLK、MISO、MOSI接一起,使用FXS引脚和一个GPIO作为片选,操作GPIO控制的片选时,需要自己模式时钟和数据吗?

Part Number: TMS320C6713B


MCBSP配置成SPI主模式和2个SPI从设备通信,这2个设备的CLK、MISO、MOSI姐一起,使用FXS引脚和一个GPIO作为片选,操作GPIO控制的片选时,需要把FXS配置成GPIO模式,将其拉高,将控制片选的GPIO拉低,这样来选中另一个设备,请问当FXS配成GPIO模式时,其他引脚也被配置成GPIO了,

此时进行SPI通信时,需要自己将CLK、 MISO、MOSI模拟出SPI的时序吗?

还是有什么其他方式能够将FXS单独配置成GPIO模式呢?