This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

swms link调用FVID2_create返回失败



您好:

    我使用dm8168 的link库,构建了link链如下:HostBitOut >> VideoBitIn >> dec(bits) >> VideoOut >> VpssIn >> swms >> disp.

    swms 使用 SYSTEM_SW_MS_SC_INST_SC5.

    但是System_linkCreate 创建swms时,提示:

    [m3vpss ] AVSYNC:WallTime IGNORE Unexpected Discontinuity.PrevTs[31341]/CurTs[167356]
 [m3vpss ] AVSYNC:WallTime IGNORE Unexpected Discontinuity.PrevTs[167356]/CurTs[197719]
 [m3vpss ]  197720: Assertion @ Line: 2129 in links_m3vpss/swMs/swMsLink_drv.c: pDrvObj->fvidHandle != NULL : failed !!!

    有人能告诉我是否有参数设置失败?或者造成这种输出的原因有哪几类?谢谢.