This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问DM368能做到3路D1信号输入,请100M网络实时视频流传输吗?



TI工程师,

你们。

我想做一个平台,连接3个视频摄像头,清晰度为D1,然后通过网络实时传输视频流到服务器。

请问DM368能做到吗?

如果可以的话,能不能支持到D3或2个D1,1个D3?或者你能提供一个最佳的方案吗?价廉物美的方案。

谢谢。