This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapl138 的ARM用starterware跑TCPIP



开发板 LogicPD,芯片omapl138,仿真器xd100V2,omapl138 的ARM用starterware跑TCPIP,用的工程是enet_echo。这个工程在arm上跑,怎么跑不起来。

  •  

    Jun,

    这是编译器的问题,如果用TI的编译器,请按下面步骤升级编译器,并使能GCC扩展功能。

    Installing the compiler

    1. Install the latest CCS 5.x from http://processors.wiki.ti.com/index.php/Download_CCS 
    2. Launch CCS -> Help -> install new software ->
    3. “Work with” - select “code generation tool updates”
    4. Check only “ARM compiler tools” v 5.0.1 or latest revision.
    5. Next -> finish

    Enabling gcc extensions

    Modify the individual build properties of all libs and examples (usblib, system, platform etc) to enable “--gcc” extension. This can be found under - ARM Compiler -> Advanced Options. Failure to do so would result in compilation errors.