This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP启动syslink出现如下问题怎么解决



Socket Created.

Socket binded to port:2012..

Socket is listening...

 Listen fd = 3.!

 ProcMgr_open.

 ProcMgr_attach.

 Attached to slave procId 0.

 ProcMgr_load.

Loaded file /app/daq.out on slave procId 0.

 Started slave procId 0.

Dsp load ok.

! Ipc_controlcmd_loadcallback finished. status = 0.

[  458.909542] <1>Assertion at Line no: 301 in /opt/ti/syslink_2_10_05_26/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Linux/IpcDrv.c: (status >= 0) : failed

 Ipc_controlcmd_startcallback finished. status = -1.

 heapSize = 42368.srHeap = 0x000d2738

Memory_alloc success for 0 process. ptr: [0x2800]. Assertion at Line no: 923 in /opt/ti/syslink_2_10_05_26/packages/ti/syslink/ipc/hlos/usr/SharedRegion.c: (id != SharedRegion_INVALIDREGIONID) : failed

 Assertion at Line no: 926 in /opt/ti/syslink_2_10_05_26/packages/ti/syslink/ipc/hlos/usr/SharedRegion.c: ( (id != SharedRegion_INVALIDREGIONID) && (id < SharedRegion_module->cfg.numEntries)) : failed

 HeapMemMP_create success for 0 processor. Handle: [0xd2718].

Notify Send to remote process 0...

Error in Notify_sendEvent: procId=1, status = 0xfffffff9

DSP启动syslink出现如下问题怎么解决