This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 U-BOOT DDR 配置 求高人指点!谢谢!

我想将u-boot从1GB(4块K4B2G1646B)修改到2GB(4块K4B4G1646B)

时序修改为796的

DMM_LISA_MAP__0~3也修改了!

修改完成之后在2GB 的ddr跑不起来,只有一个灯闪烁一下之后就没有任何反映了!

  • uboot需要关注ddr_defs_ti816x.h:

    /* For 796 MHz */
    #if defined(CONFIG_TI816X_DDR3_796)
    #define EMIF_TIM1   0x1779C9FE
    #define EMIF_TIM2   0x50608074
    #define EMIF_TIM3   0x009F857F
    #define EMIF_SDREF  0x10001841
    #define EMIF_SDCFG  0x62A73832
    #define EMIF_PHYCFG 0x00000110

    #define WR_DQS_RATIO_BYTE_LANE3 ((0x4a << 10) | 0x4a)
    #define WR_DQS_RATIO_BYTE_LANE2 ((0x4a << 10) | 0x4a)
    #define WR_DQS_RATIO_BYTE_LANE1 ((0x4a << 10) | 0x4a)
    #define WR_DQS_RATIO_BYTE_LANE0 ((0x4a << 10) | 0x4a)

    #define WR_DATA_RATIO_BYTE_LANE3 (((0x4a + 0x40) << 10) | (0x4a + 0x40))
    #define WR_DATA_RATIO_BYTE_LANE2 (((0x4a + 0x40) << 10) | (0x4a + 0x40))
    #define WR_DATA_RATIO_BYTE_LANE1 (((0x4a + 0x40) << 10) | (0x4a + 0x40))
    #define WR_DATA_RATIO_BYTE_LANE0 (((0x4a + 0x40) << 10) | (0x4a + 0x40))

    #define RD_DQS_RATIO   ((0x40 << 10) | 0x40)

    #define DQS_GATE_BYTE_LANE0  ((0x13a << 10) | 0x13a)
    #define DQS_GATE_BYTE_LANE1  ((0x13a << 10) | 0x13a)
    #define DQS_GATE_BYTE_LANE2  ((0x13a << 10) | 0x13a)
    #define DQS_GATE_BYTE_LANE3  ((0x13a << 10) | 0x13a)

     

  • 在修改完U-BOOT以后,编译的时候是否MLO也要重新再编译一次!