TMS320C6670不使用Smart Reflex电源设计咨询
我的项目对功耗设计无要求,想简化电源设计,想去掉Smart Reflex UCD9222、UCD74110和UCD74106,直接给CVDD(VDDT1、VDDT2、VDDT3)使用1.0V电压,9.75A电流,是否可行?
如果可行TMS320C6670的Smart Reflex接口VCL、VD、VCNT0、VCNT1、VCNT2、VCNT3 是否需要接10K电阻上拉到VCC1V8?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMS320C6670不使用Smart Reflex电源设计咨询
我的项目对功耗设计无要求,想简化电源设计,想去掉Smart Reflex UCD9222、UCD74110和UCD74106,直接给CVDD(VDDT1、VDDT2、VDDT3)使用1.0V电压,9.75A电流,是否可行?
如果可行TMS320C6670的Smart Reflex接口VCL、VD、VCNT0、VCNT1、VCNT2、VCNT3 是否需要接10K电阻上拉到VCC1V8?
用LM10011+LM21215A(如果电流够的话)的组合吧! 电路连接相较于UCD9222+UCD7242的组合,连接简单不少,你可以看看!缺点是LM10011是去年11月才出的比较难买。
谢谢sun的回答。
我是12V供电,还想进一步简化为非VID编程的电压转换方案,用WEBENCH做了下方案,
用LM2743给CVDD提供固定1.1V,用TPS62130给VCC1VO提供1.0V电压是否可行?
对于66X 我也是刚起步 我做的是6678的
对于6670不是很了解 不过电源这块 电压满足 电流有一定的富余 应该就没有问题了
您好!
我现在也想简化6678的电源方案,简化为非VID编程的电压转换方案
给CVDD提供固定的1.1V的电压,不知您最后做成功了吗?
非常感谢!