This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: TMS320C6748 GROUPB 1.8V电源短路

Part Number: TMS320C6748


批量生产发现TMS320C6748EZCED4 groupb上的部分电源管脚短路,拆除芯片板子不短路,测量bga底部管脚,groupb上的电源确实与gnd管脚存在短路。芯片核电使用1.28V,数字电统一使用1.84V。上电顺序符合1.28V先上,1.84V后上;电源纹波30mV以内。DSP用在收发信机上,所以收发状态下,电源轨上会叠加350MHz的射频信号,4W发射时,此信号用示波器测试峰峰值较大1VPP(测试示波器未限带宽,可能空间耦合影响测量结果)。有什么原因可能导致DSP的1.84V电源网络短路?高频干扰大有可能损坏芯片吗?

下述管脚短路

不良率大概5% 6%