您好,
C6678 在1.25GHz主频下,功耗是13.999W,请问此时芯片温度是多少呢?
有没有相关的资料?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
C6678 在1.25GHz主频下,功耗是13.999W,请问此时芯片温度是多少呢?
有没有相关的资料?
谢谢
CASPAR ZHANG:
明白你的问题了。试着回答一下。
芯片实际会达到的温度和环境温度,散热器热阻(C6678是需要使用散热器的)和芯片功耗有关。
13.999瓦是该工具打开时候的初始值,该工具当时的设置芯片壳温是85摄氏度。如果在工具初始值基础上修改温度为100度,功耗大约16瓦。
如果你的计算是芯片壳温在85摄氏度时候的功耗,就意味这你的系统热设计不应该超过85摄氏度,否则需要调整工具中的温度重新计算功耗进行热设计。
如果环境温度是30摄氏度,芯片功耗是14瓦,系统设计指标是最高85摄氏度,芯片表面到散热器(和安装有关,一般不大)加上散热器热阻应该是(85-30)/14=3.9C/W。设计中要留出充分的余量。需要散热器有不同风速下面的功耗温升曲线或热阻数据可以查。
也可以利用热仿真工具进行更加精确的估计辅助热设计。
CASPAR ZHANG,
壳温85摄氏度应该是使用散热器才能达到的,应该是你的热设计指标。环境60℃~70℃时,C6678加上散热器后的温度小于85℃,对散热器和风速要求会较高。这方面我也不是很清楚,可以联系散热器供应商。