This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMS320C6000™ DSP 具有行业领先的性能(高达 24,000 MMACS)、功效(低至 ~470mW 工作功耗/~7mW 待机功耗)、价值(1ku 数量的价格低至 6.65 美元)以及长期的 DSP 经验积累。该平台的处理和低功耗功能非常适合于影像/视频、通信和宽带基础设施、工业、医疗、测试和测量、高端计算和高性能音频等应用。简而言之,TI 提供多种浮点/定点单核和多核 DSP 选项,可解决大多数低成本或节能型应用需求所面临的大部分任务关键型设计挑战。
我认为从系统的层面来讲:C6000不仅仅是为处理单任务矩阵算法而设计,本身可以携带非常专业的DSP/BIOS多任务实时处理系统,这方面比FPGA有优势。
你可以参考IEEE上的有关使用C66x核做LTE MIMO的文章
《On matrix inversion for LTE MIMO applications using Texas Instruments floating point DSP 》