This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我想用 DM365 300Mhz 跑1080P的图像, 有点问题.



我想用 DM365 300Mhz 跑1080P的图像, 有点问题.,  发现capture是30fps,  编码是22fps左右.   

现在发现出来的图像有时候 会跳帧,   请问我改改动什么.  

我看了cpu使用率,  60%. 不到.

我修改了

#define AVSERVER_MAX_FRAMERATE (19) //change by de 30
但是 ENCODE0  |          43.63 |      22.92 |      19067 |          437 | 仍然是22.9fps, 图像有丢帧
请问问题在于前端capture 的30fps太高 还是264编码模块出现困难呢?