This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359 DP83848K 能够 link 却不能正常工作

Other Parts Discussed in Thread: DP83848K, TPS65910, AM1808, AM3359, DP83865

使用 DP83848K ,RMII 模式 ,外部 50M 晶振 ,kenel 下增加了 rmii1 pin mux 、设置了 gmii_sell 寄存器为 0xC5 、修改 slave0.phy_id 为 0x01 .

现在的状况是 可以看到 “PHY: 0:01 - Link is Up - 100/Full” ,却不能够正常工作 ,请问可能会是哪里出了错 ?

另外 ,使用的 phy 驱动为 drivers/net/phy/phy_device.c  为什么显示 “ davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown” ?

以下是 kernel 部分的所有 打印信息 ,希望大家给予指点 ,谢谢

——————————————————————————————————————————————————————————————————

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.000000] Linux version 3.2.0+ (wxy@wxy-K43SA) (gcc version 4.7.3 (Ubuntu/Linaro 4.7.3-1ubuntu1) ) #24 Wed Sep 25 11:39:35 CST 2013
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] AM335X ES1.0 (sgx neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3 rootwait ip=none
[    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Memory: 256MB = 256MB total
[    0.000000] Memory: 252888k/252888k available, 9256k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc059a000   (5704 kB)
[    0.000000]       .init : 0xc059a000 - 0xc0633000   ( 612 kB)
[    0.000000]       .data : 0xc0634000 - 0xc069e650   ( 426 kB)
[    0.000000]        .bss : 0xc069e674 - 0xc06cd424   ( 188 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[    0.000000] Console: colour dummy device 80x30
[    0.000122] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[    0.058929] pid_max: default: 32768 minimum: 301
[    0.059082] Security Framework initialized
[    0.059173] Mount-cache hash table entries: 512
[    0.059539] CPU: Testing write buffer coherency: ok
[    0.080017] omap_hwmod: pruss: failed to hardreset
[    0.081146] print_constraints: dummy:
[    0.081512] NET: Registered protocol family 16
[    0.083648] OMAP GPIO hardware version 0.1
[    0.086242] omap_mux_init: Add partition: #1: core, flags: 0
[    0.088165]  omap_i2c.1: alias fck already exists
[    0.089080]  omap2_mcspi.1: alias fck already exists
[    0.089324]  omap2_mcspi.2: alias fck already exists
[    0.090270]  edma.0: alias fck already exists
[    0.090270]  edma.0: alias fck already exists
[    0.090301]  edma.0: alias fck already exists
[    0.117065] bio: create slab <bio-0> at 0
[    0.119354] SCSI subsystem initialized
[    0.120269] --- drivers/net/phy/phy_device.c : 1036 phy_init...
[    0.120269] --- drivers/net/phy/mdio_bus.c : 391 mdio_bus_init...
[    0.120391] --- drivers/net/phy/mdio_bus.c : 395 class_register return is 0
[    0.120544] --- drivers/net/phy/mdio_bus.c : 400 bus_register return is 0
[    0.120666] --- drivers/net/phy/phy_device.c : 1046 phy_init end ,return rc is 0
[    0.121032] usbcore: registered new interface driver usbfs
[    0.121337] usbcore: registered new interface driver hub
[    0.121520] usbcore: registered new device driver usb
[    0.121826] registerd cppi-dma Intr @ IRQ 17
[    0.121826] Cppi41 Init Done Qmgr-base(d087a000) dma-base(d0878000)
[    0.121856] Cppi41 Init Done
[    0.121887] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[    0.122161] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[    0.139007] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[    0.140930] tps65910 1-002d: JTAGREVNUM 0x0
[    0.143310] print_constraints: VRTC:
[    0.144744] print_constraints: VIO: at 1500 mV
[    0.147064] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[    0.149353] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[    0.150360] print_constraints: VDD3: 5000 mV
[    0.151763] print_constraints: VDIG1: at 1800 mV
[    0.153167] print_constraints: VDIG2: at 1800 mV
[    0.154602] print_constraints: VPLL: at 1800 mV
[    0.156036] print_constraints: VDAC: at 1800 mV
[    0.157440] print_constraints: VAUX1: at 1800 mV
[    0.158874] print_constraints: VAUX2: at 3300 mV
[    0.160339] print_constraints: VAUX33: at 3300 mV
[    0.161743] print_constraints: VMMC: at 3300 mV
[    0.162261] tps65910 1-002d: No interrupt support, no core IRQ
[    0.163635] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.164794] Switching to clocksource gp timer
[    0.180236] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    0.180450] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[    0.180786] MUSB0 controller's USBSS revision = 4ea20800
[    0.181701] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using DMA, IRQ 18
[    0.181854] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[    0.182159] MUSB1 controller's USBSS revision = 4ea20800
[    0.182586] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[    0.182678] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[    0.182830] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    0.182830] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    0.182830] usb usb1: Product: MUSB HDRC host driver
[    0.182861] usb usb1: Manufacturer: Linux 3.2.0+ musb-hcd
[    0.182861] usb usb1: SerialNumber: musb-hdrc.1
[    0.183654] hub 1-0:1.0: USB hub found
[    0.183715] hub 1-0:1.0: 1 port detected
[    0.184234] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using DMA, IRQ 19
[    0.184661] NET: Registered protocol family 2
[    0.184936] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.185211] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[    0.185394] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[    0.185485] TCP: Hash tables configured (established 8192 bind 8192)
[    0.185485] TCP reno registered
[    0.185485] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.185516] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.185729] NET: Registered protocol family 1
[    0.186004] RPC: Registered named UNIX socket transport module.
[    0.186004] RPC: Registered udp transport module.
[    0.186004] RPC: Registered tcp transport module.
[    0.186035] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.186279] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.197570] VFS: Disk quotas dquot_6.5.2
[    0.197631] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.198181] msgmni has been set to 493
[    0.201324] alg: No test for stdrng (krng)
[    0.202026] io scheduler noop registered
[    0.202026] io scheduler deadline registered
[    0.202087] io scheduler cfq registered (default)
[    0.203277] Could not set LED4 to fully on
[    0.205108] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    0.874816] console [ttyO0] enabled
[    0.879119] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    0.886962] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    0.894714] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    0.902526] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    0.910308] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    0.918609] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[    0.934967] brd: module loaded
[    0.943054] loop: module loaded
[    0.946563] i2c-core: driver [tsl2550] using legacy suspend method
[    0.953033] i2c-core: driver [tsl2550] using legacy resume method
[    0.959472] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.025421] No daughter card found
[    1.029022] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    1.044189] Board name: A335����
[    1.047576] Board version: 1.5A
[    1.050842] SKU: SKU#01
[    1.053527] The board is general purpose EVM with DDR3 in profile 0
[    1.061126]  da8xx_lcdc.0: alias fck already exists
[    1.066711] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[    1.090454] Console: switching to colour frame buffer device 100x30
[    1.111236] ---arch/arm/mach-omap2/board-am335xevm.c : 1134 rmii1_init...
[    1.119232] omap-gpmc omap-gpmc: GPMC revision 6.0
[    1.124237] Registering NAND on CS0
[    1.128662]  omap_i2c.2: alias fck already exists
[    1.145477] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz
[    1.151947] tsl2550 2-0039: standard operating mode
[    1.157226] tsl2550: probe of 2-0039 failed with error -121
[    1.163452]  davinci-mcasp.1: alias fck already exists
[    1.169342]  omap_hsmmc.0: alias fck already exists
[    1.174713]  omap_hsmmc.2: alias fck already exists
[    1.180175] Configure Bluetooth Enable pin...
[    1.184722] ---arch/arm/mach-omap2/board-am335xevm.c : 805 :matrix_keypad_init...
[    1.193389] ---arch/arm/mach-omap2/board-am335xevm.c :2434 cpsw_init...
[    1.200317] ---arch/arm/mach-omap2/devices.c :1663 am33xx_cpsw_init...
[    1.207122] ---arch/arm/mach-omap2/devices.c :1668 mac_lo = 3193
[    1.213500] ---arch/arm/mach-omap2/devices.c :1669 mac_hi = 95ea1700
[    1.220214] ---arch/arm/mach-omap2/devices.c :1705 AM33XX_CPSW_MODE_RMII
[    1.227203] ---arch/arm/mach-omap2/devices.c :1722 gmii_sel = c5
[    1.234191] ---arch/arm/mach-omap2/devices.c :1756 slave0.phy_id = 0:01
[    1.241210] ---arch/arm/mach-omap2/devices.c :1757 slave1.phy_id = 0:00
[    1.248199] ---arch/arm/mach-omap2/devices.c :1758 am33xx_cpsw_init -->end...
[    1.257537] registered am33xx_sr device
[    1.264129] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.271453] omap2-nand driver initializing
[    1.276092] ONFI flash detected
[    1.279479] ONFI param page 0 valid
[    1.283111] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP)
[    1.291748] Creating 8 MTD partitions on "omap2-nand.0":
[    1.297332] 0x000000000000-0x000000020000 : "SPL"
[    1.303741] 0x000000020000-0x000000040000 : "SPL.backup1"
[    1.310699] 0x000000040000-0x000000060000 : "SPL.backup2"
[    1.317626] 0x000000060000-0x000000080000 : "SPL.backup3"
[    1.324493] 0x000000080000-0x000000260000 : "U-Boot"
[    1.331726] 0x000000260000-0x000000280000 : "U-Boot Env"
[    1.338592] 0x000000280000-0x000000780000 : "Kernel"
[    1.347137] 0x000000780000-0x000010000000 : "File System"
[    1.457244] OneNAND driver initializing
[    1.462707] CAN device driver interface
[    1.466735] CAN bus driver for Bosch D_CAN controller 1.0
[    1.473114] --- drivers/net/ethernet/ti/davinci_mdio.c :307 mdio_probe...
[    1.525451] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[    1.531890] davinci_mdio davinci_mdio.0: detected phy mask fffffffd
[    1.539123] davinci_mdio.0: probed
[    1.542694] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[    1.550384] usbcore: registered new interface driver zd1201
[    1.556427] usbcore: registered new interface driver cdc_ether
[    1.562652] usbcore: registered new interface driver cdc_eem
[    1.568725] usbcore: registered new interface driver dm9601
[    1.574584] cdc_ncm: 04-Aug-2011
[    1.578125] usbcore: registered new interface driver cdc_ncm
[    1.584014] Initializing USB Mass Storage driver...
[    1.589355] usbcore: registered new interface driver usb-storage
[    1.595642] USB Mass Storage support registered.
[    1.600860] mousedev: PS/2 mouse device common for all mice
[    1.607391] input: matrix-keypad as /devices/platform/matrix-keypad/input/input0
[    1.616394] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input1
[    1.624969] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[    1.632019] am33xx-rtc: already running
[    1.636199] i2c /dev entries driver
[    1.640472] Linux video capture interface: v2.00
[    1.645660] usbcore: registered new interface driver uvcvideo
[    1.651672] USB Video Class driver (1.1.1)
[    1.656219] lm75: probe of 2-0048 failed with error -121
[    1.716339] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.724884] cpuidle: using governor ladder
[    1.729705] cpuidle: using governor menu
[    1.737701] omap4_aes_mod_init: loading AM33X AES driver
[    1.743377] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[    1.749908] omap4_aes_probe: probe() done
[    1.754333] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[    1.760498] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[    1.772277] omap4_sham_probe: probe() done
[    1.779083] usbcore: registered new interface driver usbhid
[    1.784912] usbhid: USB HID core driver
[    1.789642] tiadc tiadc: attached adc driver
[    1.798034] usbcore: registered new interface driver snd-usb-audio
[    1.806701] _regulator_get: 2-001b supply IOVDD not found, using dummy regulator
[    1.814514] _regulator_get: 2-001b supply DVDD not found, using dummy regulator
[    1.822204] _regulator_get: 2-001b supply AVDD not found, using dummy regulator
[    1.829895] _regulator_get: 2-001b supply DRVDD not found, using dummy regulator
[    1.840362] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
[    1.851287] ALSA device list:
[    1.854400]   #0: AM335X EVM
[    1.857421] oprofile: hardware counters not available
[    1.862701] oprofile: using timer interrupt.
[    1.867187] nf_conntrack version 0.5.0 (3951 buckets, 15804 max)
[    1.873962] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.879669] TCP cubic registered
[    1.883056] NET: Registered protocol family 17
[    1.887725] can: controller area network core (rev 20090105 abi 8)
[    1.894256] NET: Registered protocol family 29
[    1.898895] can: raw protocol (rev 20090105)
[    1.903350] can: broadcast manager protocol (rev 20090105 t)
[    1.909301] Registering the dns_resolver key type
[    1.914276] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    1.922302] ThumbEE CPU extension supported.
[    1.926818] mux: Failed to setup hwmod io irq -22
[    1.932464] Power Management for AM33XX family
[    1.937347] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[    1.944000] Copied the M3 firmware to UMEM
[    1.948394] Cortex M3 Firmware Version = 0x181
[    1.954803] create_regulator: VDD1: Failed to create debugfs directory
[    1.963195] smartreflex smartreflex: am33xx_sr_probe: Driver initialized
[    1.976989] clock: disabling unused clocks to save power
[    1.995483] ---drivers/net/ethernet/ti/cpsw.c :2566 cpsw_probe...
[    2.001892] ---drivers/net/ethernet/ti/cpsw.c :2593 test_point0...
[    2.008361] Detected MACID=0:17:ea:95:93:31
[    2.012725] ---drivers/net/ethernet/ti/cpsw.c :2617 data->slaves = 2
[    2.019561] ---drivers/net/ethernet/ti/cpsw.c :2637 bus_freq_mhz = 125 mhz
[    2.027832] ---drivers/net/ethernet/ti/cpsw.c :2468 cpsw_init_slave_emac...
[    2.035125] cpsw: Detected MACID = 00:17:ea:95:93:32
[    2.040954] ---drivers/net/ethernet/ti/cpsw.c :2814 cpsw_probe end...
[    2.048889] input: gpio-keys as /devices/platform/gpio-keys/input/input2
[    2.056610] omap_rtc am33xx-rtc: setting system clock to 2013-04-05 12:21:49 UTC (1365164509)
[    2.066101] Waiting for root device /dev/mmcblk0p2...
[    2.084930] mmc0: new high speed SDHC card at address aaaa
[    2.091278] mmcblk0: mmc0:aaaa SU04G 3.69 GiB
[    2.097656]  mmcblk0: p1 p2 p3
[    2.177459] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem
[    2.184539] EXT3-fs (mmcblk0p2): write access will be enabled during recovery
[    4.377655] kjournald starting.  Commit interval 5 seconds
[    4.383453] EXT3-fs (mmcblk0p2): recovery complete
[    5.063476] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[    5.070739] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[    5.078704] Freeing init memory: 612K
INIT: version 2.88 booting
Starting udev
[    8.191284] kjournald starting.  Commit interval 5 seconds
[    8.245056] EXT3-fs (mmcblk0p3): using internal journal
[    8.250579] EXT3-fs (mmcblk0p3): recovery complete
[    8.255584] EXT3-fs (mmcblk0p3): mounted filesystem with ordered data mode
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[    8.418151] EXT3-fs (mmcblk0p2): using internal journal
ALSA: Restoring mixer settings...
Configuring network interfaces... [    8.941162] ---drivers/net/ethernet/ti/cpsw.c :1128 cpsw_slave_open...
[    8.948089] ---drivers/net/ethernet/ti/cpsw.c :1149 slave_num = 0
[    8.954528] ---drivers/net/ethernet/ti/cpsw.c :1150 slave_port = 1
[    8.961090] ---drivers/net/ethernet/ti/cpsw.c :1151 phy_id = 0:01
[    8.967529] ---drivers/net/ethernet/ti/cpsw.c :1152 rmii_en = 0
[    8.977264] --- drivers/net/phy/phy_device.c : 932 phy_probe...
[    8.983551] net eth0: CPSW phy found : id is : 0x20005c90
udhcpc (v1.20.2) started
Sending discover...
[   10.976806] PHY: 0:01 - Link is Up - 100/Full
Sending discover...
Sending discover...
No lease, failing
done.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Performing wifi calibration...
rm: can't remove '/lib/firmware/ti-connectivity/wl1271-nvs.bin': No such file or directory
Error: Module wl12xx_sdio is not currently loaded
nl80211 not found.
[   18.437774] Disabling lock debugging due to kernel taint
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
[   18.885803] ------------[ cut here ]------------
[   18.890716] WARNING: at fs/sysfs/dir.c:481 sysfs_add_one+0x88/0xa8()
[   18.897369] sysfs: cannot create duplicate filename '/bus/platform/devices/pvrsrvkm'
[   18.905456] Modules linked in: pvrsrvkm(O+) wl12xx_sdio(O)
[   18.911193] Backtrace:
[   18.913787] [<c0017cc4>] (dump_backtrace+0x0/0x10c) from [<c04151c8>] (dump_stack+0x18/0x1c)
[   18.922607]  r6:c00fc3a8 r5:00000009 r4:ce323d40 r3:c0657ecc
[   18.928558] [<c04151b0>] (dump_stack+0x0/0x1c) from [<c003f154>] (warn_slowpath_common+0x54/0x6c)
[   18.937835] [<c003f100>] (warn_slowpath_common+0x0/0x6c) from [<c003f210>] (warn_slowpath_fmt+0x38/0x40)
[   18.947784]  r8:00000001 r7:ce0ec000 r6:ce0ec000 r5:ce23a810 r4:ffffffef
[   18.954681] r3:00000009
[   18.957458] [<c003f1d8>] (warn_slowpath_fmt+0x0/0x40) from [<c00fc3a8>] (sysfs_add_one+0x88/0xa8)
[   18.966857]  r3:ce0ec000 r2:c0512a4c
[   18.970642] [<c00fc320>] (sysfs_add_one+0x0/0xa8) from [<c00fcc48>] (sysfs_do_create_link+0xf8/0x1e0)
[   18.980346]  r7:ce323d98 r6:cf013db0 r5:ce23a810 r4:ce23a900
[   18.986328] [<c00fcb50>] (sysfs_do_create_link+0x0/0x1e0) from [<c00fcd44>] (sysfs_create_link+0x14/0x18)
[   18.996398] [<c00fcd30>] (sysfs_create_link+0x0/0x18) from [<c021f790>] (bus_add_device+0xcc/0x184)
[   19.005920] [<c021f6c4>] (bus_add_device+0x0/0x184) from [<c021dafc>] (device_add+0x430/0x574)
[   19.014984]  r8:00000000 r7:c06778e0 r6:bf022b10 r5:00000000 r4:bf022b08
[   19.021881] r3:00000000
[   19.024627] [<c021d6cc>] (device_add+0x0/0x574) from [<c0221e14>] (platform_device_add+0xfc/0x1e8)
[   19.034088] [<c0221d18>] (platform_device_add+0x0/0x1e8) from [<c022214c>] (platform_device_register+0x28/0x2c)
[   19.044708]  r7:ce322000 r6:c069e680 r5:bf0249bc r4:bf022b00
[   19.050811] [<c0222124>] (platform_device_register+0x0/0x2c) from [<bf02f074>] (PVRCore_Init+0x74/0x164 [pvrsrvkm])
[   19.061828]  r4:00000000 r3:00000000
[   19.065643] [<bf02f000>] (PVRCore_Init+0x0/0x164 [pvrsrvkm]) from [<c0008764>] (do_one_initcall+0x128/0x1a8)
[   19.075897]  r5:bf022d44 r4:bf022d44
[   19.079650] [<c000863c>] (do_one_initcall+0x0/0x1a8) from [<c006be7c>] (sys_init_module+0x3e4/0x1b5c)
[   19.089324] [<c006ba98>] (sys_init_module+0x0/0x1b5c) from [<c0014640>] (ret_fast_syscall+0x0/0x30)
[   19.098754] ---[ end trace a84014b81504994a ]---
Error: could not insert module /lib/modules/3.2.0+/kernel/drivers/gpu/pvr/pvrsrvkm.ko: File exists
Could not find pvrsrvkm driver
Starting Lighttpd Web Server: lighttpd.
2013-04-05 12:22:05: (log.c.166) server started
/
Starting Matrix GUI application.
[   20.358276]  gadget: Mass Storage Function, version: 2009/09/11
[   20.364532]  gadget: Number of LUNs=2
[   20.368438]  lun0: LUN: removable file: /dev/mmcblk0p1
[   20.373840]  lun1: LUN: removable file: /dev/mmcblk0p3
[   20.379302]  gadget: Mass Storage Gadget, version: 2009/09/11
[   20.385345]  gadget: userspace failed to provide iSerialNumber
[   20.391510]  gadget: g_mass_storage ready
[   20.395751] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[   20.401428] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[   20.409332] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[   20.416473] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   20.424072] usb usb2: Product: MUSB HDRC host driver
[   20.429290] usb usb2: Manufacturer: Linux 3.2.0+ musb-hcd
[   20.434967] usb usb2: SerialNumber: musb-hdrc.0
[   20.440307] hub 2-0:1.0: USB hub found
[   20.444213] hub 2-0:1.0: 1 port detected
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
    binutils-symlinks
    binutils
    gdbserver

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.

 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project http://arago-project.org am335x-evm ttyO0

Arago 2013.02 am335x-evm ttyO0

am335x-evm login: root
root@am335x-evm:~# ifconfig
eth0      Link encap:Ethernet  HWaddr 00:17:EA:95:93:31  
          UP BROADCAST RUNNING ALLMULTI MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:644 (644.0 B)

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:16436  Metric:1
          RX packets:131 errors:0 dropped:0 overruns:0 frame:0
          TX packets:131 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:250706 (244.8 KiB)  TX bytes:250706 (244.8 KiB)