使用 DP83848K ,RMII 模式 ,外部 50M 晶振 ,kenel 下增加了 rmii1 pin mux 、设置了 gmii_sell 寄存器为 0xC5 、修改 slave0.phy_id 为 0x01 .
现在的状况是 可以看到 “PHY: 0:01 - Link is Up - 100/Full” ,却不能够正常工作 ,请问可能会是哪里出了错 ?
另外 ,使用的 phy 驱动为 drivers/net/phy/phy_device.c 为什么显示 “ davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown” ?
以下是 kernel 部分的所有 打印信息 ,希望大家给予指点 ,谢谢
——————————————————————————————————————————————————————————————————
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0+ (wxy@wxy-K43SA) (gcc version 4.7.3 (Ubuntu/Linaro 4.7.3-1ubuntu1) ) #24 Wed Sep 25 11:39:35 CST 2013
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3 rootwait ip=none
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 252888k/252888k available, 9256k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc059a000 (5704 kB)
[ 0.000000] .init : 0xc059a000 - 0xc0633000 ( 612 kB)
[ 0.000000] .data : 0xc0634000 - 0xc069e650 ( 426 kB)
[ 0.000000] .bss : 0xc069e674 - 0xc06cd424 ( 188 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000122] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.058929] pid_max: default: 32768 minimum: 301
[ 0.059082] Security Framework initialized
[ 0.059173] Mount-cache hash table entries: 512
[ 0.059539] CPU: Testing write buffer coherency: ok
[ 0.080017] omap_hwmod: pruss: failed to hardreset
[ 0.081146] print_constraints: dummy:
[ 0.081512] NET: Registered protocol family 16
[ 0.083648] OMAP GPIO hardware version 0.1
[ 0.086242] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.088165] omap_i2c.1: alias fck already exists
[ 0.089080] omap2_mcspi.1: alias fck already exists
[ 0.089324] omap2_mcspi.2: alias fck already exists
[ 0.090270] edma.0: alias fck already exists
[ 0.090270] edma.0: alias fck already exists
[ 0.090301] edma.0: alias fck already exists
[ 0.117065] bio: create slab <bio-0> at 0
[ 0.119354] SCSI subsystem initialized
[ 0.120269] --- drivers/net/phy/phy_device.c : 1036 phy_init...
[ 0.120269] --- drivers/net/phy/mdio_bus.c : 391 mdio_bus_init...
[ 0.120391] --- drivers/net/phy/mdio_bus.c : 395 class_register return is 0
[ 0.120544] --- drivers/net/phy/mdio_bus.c : 400 bus_register return is 0
[ 0.120666] --- drivers/net/phy/phy_device.c : 1046 phy_init end ,return rc is 0
[ 0.121032] usbcore: registered new interface driver usbfs
[ 0.121337] usbcore: registered new interface driver hub
[ 0.121520] usbcore: registered new device driver usb
[ 0.121826] registerd cppi-dma Intr @ IRQ 17
[ 0.121826] Cppi41 Init Done Qmgr-base(d087a000) dma-base(d0878000)
[ 0.121856] Cppi41 Init Done
[ 0.121887] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.122161] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.139007] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.140930] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.143310] print_constraints: VRTC:
[ 0.144744] print_constraints: VIO: at 1500 mV
[ 0.147064] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[ 0.149353] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.150360] print_constraints: VDD3: 5000 mV
[ 0.151763] print_constraints: VDIG1: at 1800 mV
[ 0.153167] print_constraints: VDIG2: at 1800 mV
[ 0.154602] print_constraints: VPLL: at 1800 mV
[ 0.156036] print_constraints: VDAC: at 1800 mV
[ 0.157440] print_constraints: VAUX1: at 1800 mV
[ 0.158874] print_constraints: VAUX2: at 3300 mV
[ 0.160339] print_constraints: VAUX33: at 3300 mV
[ 0.161743] print_constraints: VMMC: at 3300 mV
[ 0.162261] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.163635] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.164794] Switching to clocksource gp timer
[ 0.180236] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.180450] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.180786] MUSB0 controller's USBSS revision = 4ea20800
[ 0.181701] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using DMA, IRQ 18
[ 0.181854] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.182159] MUSB1 controller's USBSS revision = 4ea20800
[ 0.182586] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.182678] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.182830] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.182830] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.182830] usb usb1: Product: MUSB HDRC host driver
[ 0.182861] usb usb1: Manufacturer: Linux 3.2.0+ musb-hcd
[ 0.182861] usb usb1: SerialNumber: musb-hdrc.1
[ 0.183654] hub 1-0:1.0: USB hub found
[ 0.183715] hub 1-0:1.0: 1 port detected
[ 0.184234] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using DMA, IRQ 19
[ 0.184661] NET: Registered protocol family 2
[ 0.184936] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.185211] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.185394] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.185485] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.185485] TCP reno registered
[ 0.185485] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.185516] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.185729] NET: Registered protocol family 1
[ 0.186004] RPC: Registered named UNIX socket transport module.
[ 0.186004] RPC: Registered udp transport module.
[ 0.186004] RPC: Registered tcp transport module.
[ 0.186035] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.186279] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.197570] VFS: Disk quotas dquot_6.5.2
[ 0.197631] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.198181] msgmni has been set to 493
[ 0.201324] alg: No test for stdrng (krng)
[ 0.202026] io scheduler noop registered
[ 0.202026] io scheduler deadline registered
[ 0.202087] io scheduler cfq registered (default)
[ 0.203277] Could not set LED4 to fully on
[ 0.205108] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.874816] console [ttyO0] enabled
[ 0.879119] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.886962] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.894714] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.902526] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.910308] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.918609] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 0.934967] brd: module loaded
[ 0.943054] loop: module loaded
[ 0.946563] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.953033] i2c-core: driver [tsl2550] using legacy resume method
[ 0.959472] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.025421] No daughter card found
[ 1.029022] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.044189] Board name: A335����
[ 1.047576] Board version: 1.5A
[ 1.050842] SKU: SKU#01
[ 1.053527] The board is general purpose EVM with DDR3 in profile 0
[ 1.061126] da8xx_lcdc.0: alias fck already exists
[ 1.066711] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[ 1.090454] Console: switching to colour frame buffer device 100x30
[ 1.111236] ---arch/arm/mach-omap2/board-am335xevm.c : 1134 rmii1_init...
[ 1.119232] omap-gpmc omap-gpmc: GPMC revision 6.0
[ 1.124237] Registering NAND on CS0
[ 1.128662] omap_i2c.2: alias fck already exists
[ 1.145477] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz
[ 1.151947] tsl2550 2-0039: standard operating mode
[ 1.157226] tsl2550: probe of 2-0039 failed with error -121
[ 1.163452] davinci-mcasp.1: alias fck already exists
[ 1.169342] omap_hsmmc.0: alias fck already exists
[ 1.174713] omap_hsmmc.2: alias fck already exists
[ 1.180175] Configure Bluetooth Enable pin...
[ 1.184722] ---arch/arm/mach-omap2/board-am335xevm.c : 805 :matrix_keypad_init...
[ 1.193389] ---arch/arm/mach-omap2/board-am335xevm.c :2434 cpsw_init...
[ 1.200317] ---arch/arm/mach-omap2/devices.c :1663 am33xx_cpsw_init...
[ 1.207122] ---arch/arm/mach-omap2/devices.c :1668 mac_lo = 3193
[ 1.213500] ---arch/arm/mach-omap2/devices.c :1669 mac_hi = 95ea1700
[ 1.220214] ---arch/arm/mach-omap2/devices.c :1705 AM33XX_CPSW_MODE_RMII
[ 1.227203] ---arch/arm/mach-omap2/devices.c :1722 gmii_sel = c5
[ 1.234191] ---arch/arm/mach-omap2/devices.c :1756 slave0.phy_id = 0:01
[ 1.241210] ---arch/arm/mach-omap2/devices.c :1757 slave1.phy_id = 0:00
[ 1.248199] ---arch/arm/mach-omap2/devices.c :1758 am33xx_cpsw_init -->end...
[ 1.257537] registered am33xx_sr device
[ 1.264129] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.271453] omap2-nand driver initializing
[ 1.276092] ONFI flash detected
[ 1.279479] ONFI param page 0 valid
[ 1.283111] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP)
[ 1.291748] Creating 8 MTD partitions on "omap2-nand.0":
[ 1.297332] 0x000000000000-0x000000020000 : "SPL"
[ 1.303741] 0x000000020000-0x000000040000 : "SPL.backup1"
[ 1.310699] 0x000000040000-0x000000060000 : "SPL.backup2"
[ 1.317626] 0x000000060000-0x000000080000 : "SPL.backup3"
[ 1.324493] 0x000000080000-0x000000260000 : "U-Boot"
[ 1.331726] 0x000000260000-0x000000280000 : "U-Boot Env"
[ 1.338592] 0x000000280000-0x000000780000 : "Kernel"
[ 1.347137] 0x000000780000-0x000010000000 : "File System"
[ 1.457244] OneNAND driver initializing
[ 1.462707] CAN device driver interface
[ 1.466735] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.473114] --- drivers/net/ethernet/ti/davinci_mdio.c :307 mdio_probe...
[ 1.525451] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.531890] davinci_mdio davinci_mdio.0: detected phy mask fffffffd
[ 1.539123] davinci_mdio.0: probed
[ 1.542694] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[ 1.550384] usbcore: registered new interface driver zd1201
[ 1.556427] usbcore: registered new interface driver cdc_ether
[ 1.562652] usbcore: registered new interface driver cdc_eem
[ 1.568725] usbcore: registered new interface driver dm9601
[ 1.574584] cdc_ncm: 04-Aug-2011
[ 1.578125] usbcore: registered new interface driver cdc_ncm
[ 1.584014] Initializing USB Mass Storage driver...
[ 1.589355] usbcore: registered new interface driver usb-storage
[ 1.595642] USB Mass Storage support registered.
[ 1.600860] mousedev: PS/2 mouse device common for all mice
[ 1.607391] input: matrix-keypad as /devices/platform/matrix-keypad/input/input0
[ 1.616394] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input1
[ 1.624969] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 1.632019] am33xx-rtc: already running
[ 1.636199] i2c /dev entries driver
[ 1.640472] Linux video capture interface: v2.00
[ 1.645660] usbcore: registered new interface driver uvcvideo
[ 1.651672] USB Video Class driver (1.1.1)
[ 1.656219] lm75: probe of 2-0048 failed with error -121
[ 1.716339] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.724884] cpuidle: using governor ladder
[ 1.729705] cpuidle: using governor menu
[ 1.737701] omap4_aes_mod_init: loading AM33X AES driver
[ 1.743377] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.749908] omap4_aes_probe: probe() done
[ 1.754333] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.760498] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.772277] omap4_sham_probe: probe() done
[ 1.779083] usbcore: registered new interface driver usbhid
[ 1.784912] usbhid: USB HID core driver
[ 1.789642] tiadc tiadc: attached adc driver
[ 1.798034] usbcore: registered new interface driver snd-usb-audio
[ 1.806701] _regulator_get: 2-001b supply IOVDD not found, using dummy regulator
[ 1.814514] _regulator_get: 2-001b supply DVDD not found, using dummy regulator
[ 1.822204] _regulator_get: 2-001b supply AVDD not found, using dummy regulator
[ 1.829895] _regulator_get: 2-001b supply DRVDD not found, using dummy regulator
[ 1.840362] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
[ 1.851287] ALSA device list:
[ 1.854400] #0: AM335X EVM
[ 1.857421] oprofile: hardware counters not available
[ 1.862701] oprofile: using timer interrupt.
[ 1.867187] nf_conntrack version 0.5.0 (3951 buckets, 15804 max)
[ 1.873962] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.879669] TCP cubic registered
[ 1.883056] NET: Registered protocol family 17
[ 1.887725] can: controller area network core (rev 20090105 abi 8)
[ 1.894256] NET: Registered protocol family 29
[ 1.898895] can: raw protocol (rev 20090105)
[ 1.903350] can: broadcast manager protocol (rev 20090105 t)
[ 1.909301] Registering the dns_resolver key type
[ 1.914276] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.922302] ThumbEE CPU extension supported.
[ 1.926818] mux: Failed to setup hwmod io irq -22
[ 1.932464] Power Management for AM33XX family
[ 1.937347] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.944000] Copied the M3 firmware to UMEM
[ 1.948394] Cortex M3 Firmware Version = 0x181
[ 1.954803] create_regulator: VDD1: Failed to create debugfs directory
[ 1.963195] smartreflex smartreflex: am33xx_sr_probe: Driver initialized
[ 1.976989] clock: disabling unused clocks to save power
[ 1.995483] ---drivers/net/ethernet/ti/cpsw.c :2566 cpsw_probe...
[ 2.001892] ---drivers/net/ethernet/ti/cpsw.c :2593 test_point0...
[ 2.008361] Detected MACID=0:17:ea:95:93:31
[ 2.012725] ---drivers/net/ethernet/ti/cpsw.c :2617 data->slaves = 2
[ 2.019561] ---drivers/net/ethernet/ti/cpsw.c :2637 bus_freq_mhz = 125 mhz
[ 2.027832] ---drivers/net/ethernet/ti/cpsw.c :2468 cpsw_init_slave_emac...
[ 2.035125] cpsw: Detected MACID = 00:17:ea:95:93:32
[ 2.040954] ---drivers/net/ethernet/ti/cpsw.c :2814 cpsw_probe end...
[ 2.048889] input: gpio-keys as /devices/platform/gpio-keys/input/input2
[ 2.056610] omap_rtc am33xx-rtc: setting system clock to 2013-04-05 12:21:49 UTC (1365164509)
[ 2.066101] Waiting for root device /dev/mmcblk0p2...
[ 2.084930] mmc0: new high speed SDHC card at address aaaa
[ 2.091278] mmcblk0: mmc0:aaaa SU04G 3.69 GiB
[ 2.097656] mmcblk0: p1 p2 p3
[ 2.177459] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem
[ 2.184539] EXT3-fs (mmcblk0p2): write access will be enabled during recovery
[ 4.377655] kjournald starting. Commit interval 5 seconds
[ 4.383453] EXT3-fs (mmcblk0p2): recovery complete
[ 5.063476] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 5.070739] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[ 5.078704] Freeing init memory: 612K
INIT: version 2.88 booting
Starting udev
[ 8.191284] kjournald starting. Commit interval 5 seconds
[ 8.245056] EXT3-fs (mmcblk0p3): using internal journal
[ 8.250579] EXT3-fs (mmcblk0p3): recovery complete
[ 8.255584] EXT3-fs (mmcblk0p3): mounted filesystem with ordered data mode
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[ 8.418151] EXT3-fs (mmcblk0p2): using internal journal
ALSA: Restoring mixer settings...
Configuring network interfaces... [ 8.941162] ---drivers/net/ethernet/ti/cpsw.c :1128 cpsw_slave_open...
[ 8.948089] ---drivers/net/ethernet/ti/cpsw.c :1149 slave_num = 0
[ 8.954528] ---drivers/net/ethernet/ti/cpsw.c :1150 slave_port = 1
[ 8.961090] ---drivers/net/ethernet/ti/cpsw.c :1151 phy_id = 0:01
[ 8.967529] ---drivers/net/ethernet/ti/cpsw.c :1152 rmii_en = 0
[ 8.977264] --- drivers/net/phy/phy_device.c : 932 phy_probe...
[ 8.983551] net eth0: CPSW phy found : id is : 0x20005c90
udhcpc (v1.20.2) started
Sending discover...
[ 10.976806] PHY: 0:01 - Link is Up - 100/Full
Sending discover...
Sending discover...
No lease, failing
done.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Performing wifi calibration...
rm: can't remove '/lib/firmware/ti-connectivity/wl1271-nvs.bin': No such file or directory
Error: Module wl12xx_sdio is not currently loaded
nl80211 not found.
[ 18.437774] Disabling lock debugging due to kernel taint
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
[ 18.885803] ------------[ cut here ]------------
[ 18.890716] WARNING: at fs/sysfs/dir.c:481 sysfs_add_one+0x88/0xa8()
[ 18.897369] sysfs: cannot create duplicate filename '/bus/platform/devices/pvrsrvkm'
[ 18.905456] Modules linked in: pvrsrvkm(O+) wl12xx_sdio(O)
[ 18.911193] Backtrace:
[ 18.913787] [<c0017cc4>] (dump_backtrace+0x0/0x10c) from [<c04151c8>] (dump_stack+0x18/0x1c)
[ 18.922607] r6:c00fc3a8 r5:00000009 r4:ce323d40 r3:c0657ecc
[ 18.928558] [<c04151b0>] (dump_stack+0x0/0x1c) from [<c003f154>] (warn_slowpath_common+0x54/0x6c)
[ 18.937835] [<c003f100>] (warn_slowpath_common+0x0/0x6c) from [<c003f210>] (warn_slowpath_fmt+0x38/0x40)
[ 18.947784] r8:00000001 r7:ce0ec000 r6:ce0ec000 r5:ce23a810 r4:ffffffef
[ 18.954681] r3:00000009
[ 18.957458] [<c003f1d8>] (warn_slowpath_fmt+0x0/0x40) from [<c00fc3a8>] (sysfs_add_one+0x88/0xa8)
[ 18.966857] r3:ce0ec000 r2:c0512a4c
[ 18.970642] [<c00fc320>] (sysfs_add_one+0x0/0xa8) from [<c00fcc48>] (sysfs_do_create_link+0xf8/0x1e0)
[ 18.980346] r7:ce323d98 r6:cf013db0 r5:ce23a810 r4:ce23a900
[ 18.986328] [<c00fcb50>] (sysfs_do_create_link+0x0/0x1e0) from [<c00fcd44>] (sysfs_create_link+0x14/0x18)
[ 18.996398] [<c00fcd30>] (sysfs_create_link+0x0/0x18) from [<c021f790>] (bus_add_device+0xcc/0x184)
[ 19.005920] [<c021f6c4>] (bus_add_device+0x0/0x184) from [<c021dafc>] (device_add+0x430/0x574)
[ 19.014984] r8:00000000 r7:c06778e0 r6:bf022b10 r5:00000000 r4:bf022b08
[ 19.021881] r3:00000000
[ 19.024627] [<c021d6cc>] (device_add+0x0/0x574) from [<c0221e14>] (platform_device_add+0xfc/0x1e8)
[ 19.034088] [<c0221d18>] (platform_device_add+0x0/0x1e8) from [<c022214c>] (platform_device_register+0x28/0x2c)
[ 19.044708] r7:ce322000 r6:c069e680 r5:bf0249bc r4:bf022b00
[ 19.050811] [<c0222124>] (platform_device_register+0x0/0x2c) from [<bf02f074>] (PVRCore_Init+0x74/0x164 [pvrsrvkm])
[ 19.061828] r4:00000000 r3:00000000
[ 19.065643] [<bf02f000>] (PVRCore_Init+0x0/0x164 [pvrsrvkm]) from [<c0008764>] (do_one_initcall+0x128/0x1a8)
[ 19.075897] r5:bf022d44 r4:bf022d44
[ 19.079650] [<c000863c>] (do_one_initcall+0x0/0x1a8) from [<c006be7c>] (sys_init_module+0x3e4/0x1b5c)
[ 19.089324] [<c006ba98>] (sys_init_module+0x0/0x1b5c) from [<c0014640>] (ret_fast_syscall+0x0/0x30)
[ 19.098754] ---[ end trace a84014b81504994a ]---
Error: could not insert module /lib/modules/3.2.0+/kernel/drivers/gpu/pvr/pvrsrvkm.ko: File exists
Could not find pvrsrvkm driver
Starting Lighttpd Web Server: lighttpd.
2013-04-05 12:22:05: (log.c.166) server started
/
Starting Matrix GUI application.
[ 20.358276] gadget: Mass Storage Function, version: 2009/09/11
[ 20.364532] gadget: Number of LUNs=2
[ 20.368438] lun0: LUN: removable file: /dev/mmcblk0p1
[ 20.373840] lun1: LUN: removable file: /dev/mmcblk0p3
[ 20.379302] gadget: Mass Storage Gadget, version: 2009/09/11
[ 20.385345] gadget: userspace failed to provide iSerialNumber
[ 20.391510] gadget: g_mass_storage ready
[ 20.395751] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 20.401428] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 20.409332] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 20.416473] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 20.424072] usb usb2: Product: MUSB HDRC host driver
[ 20.429290] usb usb2: Manufacturer: Linux 3.2.0+ musb-hcd
[ 20.434967] usb usb2: SerialNumber: musb-hdrc.0
[ 20.440307] hub 2-0:1.0: USB hub found
[ 20.444213] hub 2-0:1.0: 1 port detected
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
binutils-symlinks
binutils
gdbserver
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyO0
Arago 2013.02 am335x-evm ttyO0
am335x-evm login: root
root@am335x-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:17:EA:95:93:31
UP BROADCAST RUNNING ALLMULTI MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:644 (644.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:131 errors:0 dropped:0 overruns:0 frame:0
TX packets:131 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:250706 (244.8 KiB) TX bytes:250706 (244.8 KiB)