This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354的DDR2和NAND-FLASH布线疑问

Other Parts Discussed in Thread: AM3354

目前选用AM3354主芯片,在DDR2和NAND-FLASH布线存在疑问,请帮忙分析:

(1)DDR布线疑问:根据DDR布线要求(网上有人说的,不知是否正确?),时钟线阻抗100ohm,其余线(控制线,地址线,数据线)阻抗55ohm,但是,我们一般会在控制线和地址线上串联33ohm电阻,那么,按照信号反射理论来讲,就存在一个问题:走线阻抗(100ohm,55ohm)与33ohm就不匹配,存在阻抗变换现象,这样就会引起信号反射?这样理解是否正确?该怎样理解?
(2)NAND-FLASH布线疑问:NAND-FLASH布线是否需要做等长?有什么要求?
  • 你好!

    (1)DDR: 阻抗匹配不是仅仅通过电阻的,还有线的阻抗。

    具体可以参考AM335X DATASSHEET中5.6.2.2 DDR2 Routing Guidelines章节

    (2)NAND FLASH:不需要很严格。

  • 1. 布线这块可以参考一下已经用的板子是怎么布线的,比如beaglebone,网上有PCB的图

    2. nand flash没啥特殊的要求把,只要布线别太离谱就行,本身的速度不高,问题不大

  • 查看了AM335X DATASSHEET中5.6.2.2 DDR2 Routing Guidelines章节,里面有个问题没有说清楚,存在一个疑问:其中要求将串联匹配电阻(典型值22ohm)靠近CPU放置,走线特征阻抗Z0(50ohm~75ohm)定义了从串联匹配电阻到DDR2的走线要求,但是,实际布线时,串联匹配电阻不可能做到完全靠近CPU,串联匹配电阻和CPU之间还存在一段走线,我的问题是:

    (1)串联匹配电阻和CPU间的走线的特征阻抗该如何要求?难道还是Z0(50ohm~75ohm吗)?

    (2)如果串联匹配电阻和CPU之间的走线的特征阻抗要求为Z0(假定为55ohm),那么整个走线(从CPU到DDR2)的特征阻抗是不是55ohm---22ohm--55ohm了呢?那这样的话,岂不是阻抗发生了变化,会导致信号反射吗?

    请老师帮忙解答,非常感谢!!

  • 区分电阻和阻抗