目前选用AM3354主芯片,在DDR2和NAND-FLASH布线存在疑问,请帮忙分析:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前选用AM3354主芯片,在DDR2和NAND-FLASH布线存在疑问,请帮忙分析:
查看了AM335X DATASSHEET中5.6.2.2 DDR2 Routing Guidelines章节,里面有个问题没有说清楚,存在一个疑问:其中要求将串联匹配电阻(典型值22ohm)靠近CPU放置,走线特征阻抗Z0(50ohm~75ohm)定义了从串联匹配电阻到DDR2的走线要求,但是,实际布线时,串联匹配电阻不可能做到完全靠近CPU,串联匹配电阻和CPU之间还存在一段走线,我的问题是:
(1)串联匹配电阻和CPU间的走线的特征阻抗该如何要求?难道还是Z0(50ohm~75ohm吗)?
(2)如果串联匹配电阻和CPU之间的走线的特征阻抗要求为Z0(假定为55ohm),那么整个走线(从CPU到DDR2)的特征阻抗是不是55ohm---22ohm--55ohm了呢?那这样的话,岂不是阻抗发生了变化,会导致信号反射吗?
请老师帮忙解答,非常感谢!!