This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320C6474 中SRIO port和serdes配置问题的请教



hi,在TMS320C6474的SRIO UG中介绍,共有两个port,且serdes的配置如下:

Table 60. SERDES_CFGRXn_CNTL Registers and the Associated Ports
Register                                                            Address                              Offset Associated Port
SERDES_CFGRX0_CNTL                            0100h                                  Port 0
SERDES_CFGRX1_CNTL                            0104h                                  Port 1

可在SRIO的的例程中配置了四个,具体如下:

    hSrio->regs->SERDES_CFG_CNTL[0]   = 0x0;
    hSrio->regs->SERDES_CFG_CNTL[1]   = 0x0;
    hSrio->regs->SERDES_CFG_CNTL[2]   = 0x0;
    hSrio->regs->SERDES_CFG_CNTL[3]   = 0x0;

   在include的头文件cslr_srio.h中关于寄存器的结构体成员中定义也为四个,具体如下:

 volatile Uint32 SERDES_CFGRX_CNTL[4];

也就是说,这个device共有两个port,对应的serdes也有两个,配置也应该是两个,可是为什么例程中却配置了4个,且头文件中也为4个?编译也没问题。

对此有些困惑,请指教。

谢谢!