Other Parts Discussed in Thread: TMS320C6474
hi,在TMS320C6474的SRIO UG中介绍,共有两个port,且serdes的配置如下:
Table 60. SERDES_CFGRXn_CNTL Registers and the Associated Ports
Register Address Offset Associated Port
SERDES_CFGRX0_CNTL 0100h Port 0
SERDES_CFGRX1_CNTL 0104h Port 1
可在SRIO的的例程中配置了四个,具体如下:
hSrio->regs->SERDES_CFG_CNTL[0] = 0x0;
hSrio->regs->SERDES_CFG_CNTL[1] = 0x0;
hSrio->regs->SERDES_CFG_CNTL[2] = 0x0;
hSrio->regs->SERDES_CFG_CNTL[3] = 0x0;
在include的头文件cslr_srio.h中关于寄存器的结构体成员中定义也为四个,具体如下:
volatile Uint32 SERDES_CFGRX_CNTL[4];
也就是说,这个device共有两个port,对应的serdes也有两个,配置也应该是两个,可是为什么例程中却配置了4个,且头文件中也为4个?编译也没问题。
对此有些困惑,请指教。
谢谢!