This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM365不用PRTCSS功能

TMS320DM365不用PRTCSS功能,所有PRTCSS功能的引脚怎么连接,是否可以悬空
?????????????? 

  • 你好,

    PRTCSS Reset and Configuration里面的normal mode不使用,至少会使用external reset mode。

    RTC不使用,时钟脚在数据手册上有提到不使用情况的配置。

    其他GPIO不使用,如果默认是输入需要上拉或者下拉给一个固定电平。输出脚可以悬空。这点对于其他不使用引脚是通用的。

  • 1.至少会使用external reset mode引脚是哪个??

    2.RTC不使用,时钟脚在数据手册上有提到不使用情况的配置

    数据手册我怎么没看到啊??能详细告诉我详细的内容在哪页吗??

  • 你好,

    1. 请下载PRTCSS user guide,参考相关章节。

    2. 请参考数据手册(SPRS457E–MARCH 2009–REVISED JUNE 2011)第42页:

    RTCXI G1 I PRTCS VDD12_PRTCSS Input PRTCSS: Crystal Input for PRTCSS oscillator
    S Note: If the RTC calendar is not used, this pin should
    be pulled down.
    For more pin termination details, see Section 6.7,
    Power Management and Real Time Clock
    Subsystem (PRTCSS).

    RTCXO H1 O PRTCS VDD12_PRTCSS Output PRTCSS: Crystal Output for PRTCSS oscillator
    S Note: If the RTC calendar is not used, this pin should
    be left unconnected.
    For more pin termination details, see Section 6.7,
    Power Management and Real Time Clock
    Subsystem (PRTCSS).

  • 给个以上文档的链接吧!我找了半天没找到啊!!谢谢了!!

  • 找到了呵呵谢谢啊