TMS320DM365不用PRTCSS功能,所有PRTCSS功能的引脚怎么连接,是否可以悬空
??????????????
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMS320DM365不用PRTCSS功能,所有PRTCSS功能的引脚怎么连接,是否可以悬空
??????????????
你好,
PRTCSS Reset and Configuration里面的normal mode不使用,至少会使用external reset mode。
RTC不使用,时钟脚在数据手册上有提到不使用情况的配置。
其他GPIO不使用,如果默认是输入需要上拉或者下拉给一个固定电平。输出脚可以悬空。这点对于其他不使用引脚是通用的。
1.至少会使用external reset mode引脚是哪个??
2.RTC不使用,时钟脚在数据手册上有提到不使用情况的配置
数据手册我怎么没看到啊??能详细告诉我详细的内容在哪页吗??
你好,
1. 请下载PRTCSS user guide,参考相关章节。
2. 请参考数据手册(SPRS457E–MARCH 2009–REVISED JUNE 2011)第42页:
RTCXI G1 I PRTCS VDD12_PRTCSS Input PRTCSS: Crystal Input for PRTCSS oscillator
S Note: If the RTC calendar is not used, this pin should
be pulled down.
For more pin termination details, see Section 6.7,
Power Management and Real Time Clock
Subsystem (PRTCSS).
RTCXO H1 O PRTCS VDD12_PRTCSS Output PRTCSS: Crystal Output for PRTCSS oscillator
S Note: If the RTC calendar is not used, this pin should
be left unconnected.
For more pin termination details, see Section 6.7,
Power Management and Real Time Clock
Subsystem (PRTCSS).