大家在用ImageTuningTool调试新的sensor IMX122,有几个问题麻烦大家帮忙解答下,
1、都需要那几种光源?我现在使用D65、D50、TL84、F四种,是不是还需要D75?
2、室外的AWB是如何处理的?
3、摄像头对准室外的时候有局部过爆的情况,需要怎么调试?
谢谢大家。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家在用ImageTuningTool调试新的sensor IMX122,有几个问题麻烦大家帮忙解答下,
1、都需要那几种光源?我现在使用D65、D50、TL84、F四种,是不是还需要D75?
2、室外的AWB是如何处理的?
3、摄像头对准室外的时候有局部过爆的情况,需要怎么调试?
谢谢大家。
你好,
1,光源建议4种或者以上,选择符合热辐射原理的光源。
2. D65就是白天室外的光源模拟。
3. 这是AE的处理,和AWB无关。
谢谢,chris
关于3,AE调整需要如何操作?目前看代码上的关系没有理出头绪。
我调整了targetbrightness之后,室外就过曝了,然后我又降低了minexposure和maxexposure,这时图像闪烁的很厉害,我想可能和stepsize有关,这个参数应该和曝光时间有关吧,如何计算呢?