This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 AWB调试

大家在用ImageTuningTool调试新的sensor IMX122,有几个问题麻烦大家帮忙解答下,

1、都需要那几种光源?我现在使用D65、D50、TL84、F四种,是不是还需要D75?

2、室外的AWB是如何处理的?

3、摄像头对准室外的时候有局部过爆的情况,需要怎么调试?

谢谢大家。

  • 你好,

    1,光源建议4种或者以上,选择符合热辐射原理的光源。

    2. D65就是白天室外的光源模拟。

    3. 这是AE的处理,和AWB无关。

  • 谢谢,chris

    关于3,AE调整需要如何操作?目前看代码上的关系没有理出头绪。

    我调整了targetbrightness之后,室外就过曝了,然后我又降低了minexposure和maxexposure,这时图像闪烁的很厉害,我想可能和stepsize有关,这个参数应该和曝光时间有关吧,如何计算呢?