This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于更换dm368上的摄像头的问题

Other Parts Discussed in Thread: TVP5146, TVP7002

大家好:

      小弟我在ti-dvsdk_dm368-evm_4_02_00_06上做开发应用,现在不想用原有的MT9P031的Sensor了,换了一个OV系列的Sensor,sensor自带ISP,能出YUV420和YUV422的数据,但是不知道怎么把senor加到dm368上,看别人说可以通过修改tvp5146.c的驱动,添加YUV的sensor,然后我就把sensor的初始化寄存器配置添加在tvp5146.c里面了,然后通过运行 encode -V /111.264  -I 4 -y 2 -w 来获取视频,最后发现说我的pixformat有错,encode就运行不了;后来,我又在tvp7002.c里面加,encode是运行起来了,但是一直得不到数据,存下来的视频文件大小一直就是0!    很是纠结啊  现在都不知道添加yuv的sensor的路子是不是走对了,跪求高手啊

  • 从TVP7002驱动来改是正确的思路。 这边你需要隔离定位一下看是Sensor没有配置对还是说368这边采集没有设置对。

    你先看看sensor这边有没有设置正确:

    1.通过配置线去回读sensor的状态寄存器或者看有没有配置正确,sensor有没有跑起来,向外面输出图像;

    2. 测量sensor对外输出的信号,看有没有时钟/同步/数据信号

    3. 配置sensor输出colorbar或者其他test pattern,并修改sensor输出的格式,看能不能采集到任何图像

  • 感谢您的回答,sensor的配置是没有问题的,应该是dm368哪儿没有配好,后来我转到 IPNC 上就OK了