This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ARM(Cortex A9)与DSP(TMS320C6657)通讯方式的咨询。



        有个产品设计需求,要求ARM与DSP之间进行时大数据量通讯,通讯速率要求在80Mb/s以上,查阅了相关技术资料,通讯方式有以下几种,具体选哪种通讯方式更好的一点呢,或者大家有更好的建议,也可以分享下,主要从设计开发难度来考量。

1、HPI接口:早期ARM与DSP通讯主流接口方式,中、低端DSP处理器
       有HPI接口,参考开发资料较详细,对应DSP处理器性能一般,无法满足性能要求。
2、双口RAM:DSP与ARM共用内存单元,即采用双口RAM器件,DSP与ARM共用内存器件,ARM与DSP之间通讯速率高,设计实现不知是否容易。
3、EMIF转USB:USB通信是我们目前板级通讯比较常用的通讯接口,通讯速率没问题,DSP本身不配备USB接口,有一种通过EMIF总线转出USB接口,然后通过USB与ARM通讯,开发难点在DSP上固件的实现。
4、HS-SPI:高速串行总线,Tx和Rx频率最高可以到50Mhz,ARM与DSP均有此通讯接口,但能否满足图像传输的实时性要求需要评估。
5、以太网:通讯速率没问题,ARM与DSP均有此通讯接口,已经实现了。但板内通讯较少采用以太网方式。

请大家做过类似设计开发的大神给些意见,谢谢。本人QQ:164414905 

  • 1. 如果对ARM要求不高,可以采用集成SoC方案,TI有多款产品供客户选择。

    2. 采用分立方案的话EMIF加双口RAM实现较为简单,但是速率可能不满足要求

    3. ARM和DSP之间如果有GE口是可以SERDES直连的,不需要PHY的介入,这种设计在通信类产品中很常见。