This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 about i2c driver



Hello specialist:

       I now have used dm6467 platform.i want to  acheve i2c as slave driver,while i know  it 's as master in the most of time for linux os. I want to use it as slave device,can be used  External devices as master. how to do it?

regards

                       Leo

 

  • 我中文说吧,我现在的方案中 DM6467作为从机要和外部的主机通信,通过I2C,我看了6467的I2C linux驱动似乎只支持dm6467作为主机,然后我现在绕过驱动,直接操作寄存器初始化为从机,初始化部分有什么问题麻烦看一下:

    然后

    void i2c_init(int speed, int slaveadd)

    {

    u_int32_t div, psc;

    /*

    step 1

    ICMDR-IRS  

    clear IRS=0;

    */

    REG(I2C_CON) = 0;

    usleep(80000);

    printf("I2c--->Reset: [0x%lx] \n",REG(I2C_CON));

    /*

    step2

    ICMDR-XA

    set xa for 7bit adress

    */

    REG(I2C_OA) = slaveadd;

    REG(I2C_SA) =slaveadd;

    printf("I2c--->Slave: [0x%lx] \n",REG(I2C_OA));

    REG(I2C_CNT) =0;

    /*

    step3

    ICIMR AAS=1 ICRRDY=1 ICXRDY=1 SCD=1

    set interrupt bit

    */

    /* Interrupts must be enabled or I2C module won't work */

    REG(I2C_IE) = I2C_IE_SCD_IE | I2C_IE_XRDY_IE |

         I2C_IE_RRDY_IE |I2C_IE_AAS_IE ;

    printf("I2c--->IE: [0x%lx] \n",REG(I2C_IE));

    /*

    step4

                        CONFIG_SYS_HZ_CLOCK  =990M;

                        speed=400Hz (主要是主机是模拟的)

    */

    psc = 8;

    div = (CONFIG_SYS_HZ_CLOCK / ((psc + 1) * speed)) - 10;

    printf("div: %d \n",div);

    REG(I2C_PSC) = psc;

    REG(I2C_SCLL) = (div * 50) / 100;

    REG(I2C_SCLH) = div - REG(I2C_SCLL);

    /*

    step5

    ICMDR MST=0 FDF=0 BC=0 DLB=0 STB=0 RM=1 STP=0 STT=1

    set mod register

    */

    /* Now enable I2C controller (get it out of reset) */

    REG(I2C_CON) = I2C_CON_RM | I2C_CON_STT ;

    REG(I2C_CON) = I2C_CON_EN | REG(I2C_CON);

    printf("I2c--->MDR: [0x%lx] \n",REG(I2C_CON));

    }

  • 我中文说吧,我现在的方案中 DM6467作为从机要和外部的主机通信,通过I2C,我看了6467的I2C linux驱动似乎只支持dm6467作为主机,然后我现在绕过驱动,直接操作寄存器初始化为从机,初始化部分有什么问题麻烦看一下:

    然后

    void i2c_init(int speed, int slaveadd)

    {

    u_int32_t div, psc;

    /*

    step 1

    ICMDR-IRS  

    clear IRS=0;

    */

    REG(I2C_CON) = 0;

    usleep(80000);

    printf("I2c--->Reset: [0x%lx] \n",REG(I2C_CON));

    /*

    step2

    ICMDR-XA

    set xa for 7bit adress

    */

    REG(I2C_OA) = slaveadd;

    REG(I2C_SA) =slaveadd;

    printf("I2c--->Slave: [0x%lx] \n",REG(I2C_OA));

    REG(I2C_CNT) =0;

    /*

    step3

    ICIMR AAS=1 ICRRDY=1 ICXRDY=1 SCD=1

    set interrupt bit

    */

    /* Interrupts must be enabled or I2C module won't work */

    REG(I2C_IE) = I2C_IE_SCD_IE | I2C_IE_XRDY_IE |

         I2C_IE_RRDY_IE |I2C_IE_AAS_IE ;

    printf("I2c--->IE: [0x%lx] \n",REG(I2C_IE));

    /*

    step4

                        CONFIG_SYS_HZ_CLOCK  =990M;

                        speed=400Hz (主要是主机是模拟的)

    */

    psc = 8;

    div = (CONFIG_SYS_HZ_CLOCK / ((psc + 1) * speed)) - 10;

    printf("div: %d \n",div);

    REG(I2C_PSC) = psc;

    REG(I2C_SCLL) = (div * 50) / 100;

    REG(I2C_SCLH) = div - REG(I2C_SCLL);

    /*

    step5

    ICMDR MST=0 FDF=0 BC=0 DLB=0 STB=0 RM=1 STP=0 STT=1

    set mod register

    */

    /* Now enable I2C controller (get it out of reset) */

    REG(I2C_CON) = I2C_CON_RM | I2C_CON_STT ;

    REG(I2C_CON) = I2C_CON_EN | REG(I2C_CON);

    printf("I2c--->MDR: [0x%lx] \n",REG(I2C_CON));

    }