Hello specialist:
I now have used dm6467 platform.i want to acheve i2c as slave driver,while i know it 's as master in the most of time for linux os. I want to use it as slave device,can be used External devices as master. how to do it?
regards
Leo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hello specialist:
I now have used dm6467 platform.i want to acheve i2c as slave driver,while i know it 's as master in the most of time for linux os. I want to use it as slave device,can be used External devices as master. how to do it?
regards
Leo
1. sure , plz. check www.ti.com/.../spruer0d.pdf
我中文说吧,我现在的方案中 DM6467作为从机要和外部的主机通信,通过I2C,我看了6467的I2C linux驱动似乎只支持dm6467作为主机,然后我现在绕过驱动,直接操作寄存器初始化为从机,初始化部分有什么问题麻烦看一下:
然后
void i2c_init(int speed, int slaveadd)
{
u_int32_t div, psc;
/*
step 1
ICMDR-IRS
clear IRS=0;
*/
REG(I2C_CON) = 0;
usleep(80000);
printf("I2c--->Reset: [0x%lx] \n",REG(I2C_CON));
/*
step2
ICMDR-XA
set xa for 7bit adress
*/
REG(I2C_OA) = slaveadd;
REG(I2C_SA) =slaveadd;
printf("I2c--->Slave: [0x%lx] \n",REG(I2C_OA));
REG(I2C_CNT) =0;
/*
step3
ICIMR AAS=1 ICRRDY=1 ICXRDY=1 SCD=1
set interrupt bit
*/
/* Interrupts must be enabled or I2C module won't work */
REG(I2C_IE) = I2C_IE_SCD_IE | I2C_IE_XRDY_IE |
I2C_IE_RRDY_IE |I2C_IE_AAS_IE ;
printf("I2c--->IE: [0x%lx] \n",REG(I2C_IE));
/*
step4
CONFIG_SYS_HZ_CLOCK =990M;
speed=400Hz (主要是主机是模拟的)
*/
psc = 8;
div = (CONFIG_SYS_HZ_CLOCK / ((psc + 1) * speed)) - 10;
printf("div: %d \n",div);
REG(I2C_PSC) = psc;
REG(I2C_SCLL) = (div * 50) / 100;
REG(I2C_SCLH) = div - REG(I2C_SCLL);
/*
step5
ICMDR MST=0 FDF=0 BC=0 DLB=0 STB=0 RM=1 STP=0 STT=1
set mod register
*/
/* Now enable I2C controller (get it out of reset) */
REG(I2C_CON) = I2C_CON_RM | I2C_CON_STT ;
REG(I2C_CON) = I2C_CON_EN | REG(I2C_CON);
printf("I2c--->MDR: [0x%lx] \n",REG(I2C_CON));
}
我中文说吧,我现在的方案中 DM6467作为从机要和外部的主机通信,通过I2C,我看了6467的I2C linux驱动似乎只支持dm6467作为主机,然后我现在绕过驱动,直接操作寄存器初始化为从机,初始化部分有什么问题麻烦看一下:
然后
void i2c_init(int speed, int slaveadd)
{
u_int32_t div, psc;
/*
step 1
ICMDR-IRS
clear IRS=0;
*/
REG(I2C_CON) = 0;
usleep(80000);
printf("I2c--->Reset: [0x%lx] \n",REG(I2C_CON));
/*
step2
ICMDR-XA
set xa for 7bit adress
*/
REG(I2C_OA) = slaveadd;
REG(I2C_SA) =slaveadd;
printf("I2c--->Slave: [0x%lx] \n",REG(I2C_OA));
REG(I2C_CNT) =0;
/*
step3
ICIMR AAS=1 ICRRDY=1 ICXRDY=1 SCD=1
set interrupt bit
*/
/* Interrupts must be enabled or I2C module won't work */
REG(I2C_IE) = I2C_IE_SCD_IE | I2C_IE_XRDY_IE |
I2C_IE_RRDY_IE |I2C_IE_AAS_IE ;
printf("I2c--->IE: [0x%lx] \n",REG(I2C_IE));
/*
step4
CONFIG_SYS_HZ_CLOCK =990M;
speed=400Hz (主要是主机是模拟的)
*/
psc = 8;
div = (CONFIG_SYS_HZ_CLOCK / ((psc + 1) * speed)) - 10;
printf("div: %d \n",div);
REG(I2C_PSC) = psc;
REG(I2C_SCLL) = (div * 50) / 100;
REG(I2C_SCLH) = div - REG(I2C_SCLL);
/*
step5
ICMDR MST=0 FDF=0 BC=0 DLB=0 STB=0 RM=1 STP=0 STT=1
set mod register
*/
/* Now enable I2C controller (get it out of reset) */
REG(I2C_CON) = I2C_CON_RM | I2C_CON_STT ;
REG(I2C_CON) = I2C_CON_EN | REG(I2C_CON);
printf("I2c--->MDR: [0x%lx] \n",REG(I2C_CON));
}