This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368监控摄像机

Other Parts Discussed in Thread: TPS650061

专家,你好:

我想用DM368芯片设计一款IPCamera,参数要求如下:

1、3M以上镜头(包含);

2、1080P@30fps;

3、Ethernet;

4、DDR2-128M;

5、NAND-128M;

6、TPS650061;

 

请问专家上面的参数要求能实现吗,设计上有问题吗?

请推荐一下各器件的型号(最好TI已经有驱动),方便的话,请把相关资料、源码、参考设计发一下。

 

 

问题2:

看了DM368的数据手册,看到一个疑惑点:

就是当DM368在HD(1080P,不显示,视频数据直接通过Ethernet输出)时,ARM926必须工作在432MHz,同时Vedio Encode必须工作在74.25MHz吗?

好像PLLs是无法同时产生432MHz和74.25MHz的,专家,有什么较低成本的方案吗?