Part Number: SK-TDA4VM
请问ti-processor-sdk-linux-j7-evm-08_04_00_11这个版本的sdk可以捕获raw16的图片吗,我看j721e-csi2rx.c文件里的ti_csi2rx_fmt里面没有raw16的相关结构体
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请参考以下回复:
it could be easily added in the struct static const struct ti_csi2rx_fmt formats[ ] available in j721e-csi2rx driver.
The same is mentioned at the end of this struct "More formats can be supported but they are not listed for now"
您好,
您添加的方式是没问题的。
您能否确认这个更改有没有反映在"media/ctl -p "中?
我们这边能否获取相同 media/ctl -p 的log以及application logs?
您好,这是media ctl -p的内容
Media controller API version 5.10.120
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:4500000.ticsi2rx
hw revision 0x1
driver version 5.10.120
Device topology
- entity 1: 4500000.ticsi2rx (17 pads, 17 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
<- "cdns_csi2rx.4504000.csi-bridge":1 [ENABLED,IMMUTABLE]
pad1: Source
-> "4500000.ticsi2rx context 0":0 [ENABLED,IMMUTABLE]
pad2: Source
-> "4500000.ticsi2rx context 1":0 [ENABLED,IMMUTABLE]
pad3: Source
-> "4500000.ticsi2rx context 2":0 [ENABLED,IMMUTABLE]
pad4: Source
-> "4500000.ticsi2rx context 3":0 [ENABLED,IMMUTABLE]
pad5: Source
-> "4500000.ticsi2rx context 4":0 [ENABLED,IMMUTABLE]
pad6: Source
-> "4500000.ticsi2rx context 5":0 [ENABLED,IMMUTABLE]
pad7: Source
-> "4500000.ticsi2rx context 6":0 [ENABLED,IMMUTABLE]
pad8: Source
-> "4500000.ticsi2rx context 7":0 [ENABLED,IMMUTABLE]
pad9: Source
-> "4500000.ticsi2rx context 8":0 [ENABLED,IMMUTABLE]
pad10: Source
-> "4500000.ticsi2rx context 9":0 [ENABLED,IMMUTABLE]
pad11: Source
-> "4500000.ticsi2rx context 10":0 [ENABLED,IMMUTABLE]
pad12: Source
-> "4500000.ticsi2rx context 11":0 [ENABLED,IMMUTABLE]
pad13: Source
-> "4500000.ticsi2rx context 12":0 [ENABLED,IMMUTABLE]
pad14: Source
-> "4500000.ticsi2rx context 13":0 [ENABLED,IMMUTABLE]
pad15: Source
-> "4500000.ticsi2rx context 14":0 [ENABLED,IMMUTABLE]
pad16: Source
-> "4500000.ticsi2rx context 15":0 [ENABLED,IMMUTABLE]
- entity 19: cdns_csi2rx.4504000.csi-bridge (5 pads, 2 links, 0 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev1
pad0: Sink
<- "imx219 8-0010":0 [ENABLED,IMMUTABLE]
pad1: Source
-> "4500000.ticsi2rx":0 [ENABLED,IMMUTABLE]
pad2: Source
pad3: Source
pad4: Source
- entity 25: imx219 8-0010 (1 pad, 1 link, 0 route)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev2
pad0: Source
[stream:0 fmt:SBGGR16_1X16/3856x2177 field:none
crop.bounds:(0,0)/0x0
crop:(0,0)/0x0
compose.bounds:(0,0)/0x0
compose:(0,0)/0x0]
-> "cdns_csi2rx.4504000.csi-bridge":0 [ENABLED,IMMUTABLE]
- entity 31: 4500000.ticsi2rx context 0 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video2
pad0: Sink
<- "4500000.ticsi2rx":1 [ENABLED,IMMUTABLE]
- entity 37: 4500000.ticsi2rx context 1 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video3
pad0: Sink
<- "4500000.ticsi2rx":2 [ENABLED,IMMUTABLE]
- entity 43: 4500000.ticsi2rx context 2 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video4
pad0: Sink
<- "4500000.ticsi2rx":3 [ENABLED,IMMUTABLE]
- entity 49: 4500000.ticsi2rx context 3 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video5
pad0: Sink
<- "4500000.ticsi2rx":4 [ENABLED,IMMUTABLE]
- entity 55: 4500000.ticsi2rx context 4 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video6
pad0: Sink
<- "4500000.ticsi2rx":5 [ENABLED,IMMUTABLE]
- entity 61: 4500000.ticsi2rx context 5 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video7
pad0: Sink
<- "4500000.ticsi2rx":6 [ENABLED,IMMUTABLE]
- entity 67: 4500000.ticsi2rx context 6 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video8
pad0: Sink
<- "4500000.ticsi2rx":7 [ENABLED,IMMUTABLE]
- entity 73: 4500000.ticsi2rx context 7 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video9
pad0: Sink
<- "4500000.ticsi2rx":8 [ENABLED,IMMUTABLE]
- entity 79: 4500000.ticsi2rx context 8 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video10
pad0: Sink
<- "4500000.ticsi2rx":9 [ENABLED,IMMUTABLE]
- entity 85: 4500000.ticsi2rx context 9 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video11
pad0: Sink
<- "4500000.ticsi2rx":10 [ENABLED,IMMUTABLE]
- entity 91: 4500000.ticsi2rx context 10 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video12
pad0: Sink
<- "4500000.ticsi2rx":11 [ENABLED,IMMUTABLE]
- entity 97: 4500000.ticsi2rx context 11 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video13
pad0: Sink
<- "4500000.ticsi2rx":12 [ENABLED,IMMUTABLE]
- entity 103: 4500000.ticsi2rx context 12 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video14
pad0: Sink
<- "4500000.ticsi2rx":13 [ENABLED,IMMUTABLE]
- entity 109: 4500000.ticsi2rx context 13 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video15
pad0: Sink
<- "4500000.ticsi2rx":14 [ENABLED,IMMUTABLE]
- entity 115: 4500000.ticsi2rx context 14 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video16
pad0: Sink
<- "4500000.ticsi2rx":15 [ENABLED,IMMUTABLE]
- entity 121: 4500000.ticsi2rx context 15 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video17
pad0: Sink
<- "4500000.ticsi2rx":16 [ENABLED,IMMUTABLE]
-------------------------------------------------------------------------------------------------------------------------------------------
关于application logs,从sensor驱动上看,在发送完sensor的出流命令后,就阻塞了,没有打印任何错误信息。
我在j721e-csi2rx.c里的ti_csi2rx_dma_callback函数里加了打印,也没有正常触发
我量了设备上的mipi触点,是有正常在发送mipi信号的
我是使用了v4l2的API启动stream。

用yavta会报错

cam我使用的是imx728,是通过修改imx219的驱动实现的,当我加载imx728的raw12配置时,是能正常抓取到图片的。
这是从传感器或 CSI Rx DPHY MIPI 通道发送的数据,是可以在该通道上看到数据?
是从sensor发送进入SK-TDA4VM之前,我通过示波器量取到的,发送端看起来没问题。
请问您那能尝试raw16接收吗,因为之前我论坛里是有人回复我,能接收raw16格式的,您那有相应的sensor可以尝试吗?
如果您那能成功获取到,我就会去找自己发送端的问题